Hi,
This typo existed at least from PSDKR v8.0 to v8.5,
And BTW, shouln't we add an GT_trace8() API? Since 8 bytes is very convenient to trace memory or numbers in 64 bits. Currently only GT_trace7() is suported.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This typo existed at least from PSDKR v8.0 to v8.5,
And BTW, shouln't we add an GT_trace8() API? Since 8 bytes is very convenient to trace memory or numbers in 64 bits. Currently only GT_trace7() is suported.
Hi Keelung Yang,
Thanks for pointing this out. i have raised this bug to team, https://jira.itg.ti.com/browse/PDK-12474. Will try to get it fixed.
Please note that these are number of parameters, not the size of each parameter. I really doubt there is any API with more than 7 parameters, but yes, this can be easily added if required.
Regards,
Brijesh