This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCZAD: What I want to achieve with TM4C129ENCZAD

Part Number: TM4C129ENCZAD
Other Parts Discussed in Thread: AWR1843

I would like to drive the TM4C129ENCZAD on my custom board for the following purposes.

1. Convert USB signal to UART to communicate with other target.
2. Convert USB signals to JTAG signals to communicate with other ICs.
3. Display on the COM port when connected via USB. (Windows)
4. Drive as a USB device

Is it possible to create this by editing the program ourselves?
Also, which SDK for Tiva Ware should I refer to when making it?