Hello Champs,
HW: tda4ve j721s2
Customer can use the camera on SDK 8.4 successfully.
But when he upgrades to 8.5 SDK version. It prompts below error message when running the camera.
App Create Graph Done!
832.018575 s: VX_ZONE_ERROR:[ownContextSendCmd:802] Command ack message returned failure cmd_status: -1
832.018627 s: VX_ZONE_ERROR:[ownContextSendCmd:838] tivxEventWait() failed.
832.018635 s: VX_ZONE_ERROR:[ownNodeKernelInit:525] Target kernel, TIVX_CMD_NODE_CREATE failed for node capture_node
832.018642 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Please be sure the target callbacks have been registered for this core
832.018648 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
832.019155 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.capture ... failed !!!
832.019169 s: VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed
832.019175 s: VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed
[MCU2_0] 832.017828 s: [UDMA]
[MCU2_0] 832.017867 s: [Error] RM PSI Pairing failed!!!
[MCU2_0] 832.017893 s: [UDMA]
[MCU2_0] 832.017919 s: [Error] UDMA channel paring failed!!
[MCU2_0] 832.017964 s: src/csirx_drvUdma.c @ Line 246:
[MCU2_0] 832.017990 s: [ERROR]UDMA channel open FAILED!!!
[MCU2_0] 832.018024 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018049 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018080 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018104 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018133 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018156 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018186 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018209 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018238 s: src/csirx_drv.c @ Line 402:
[MCU2_0] 832.018262 s: Create failed for given configuration
[MCU2_0] 832.018294 s: src/fvid2_drvMgr.c @ Line 759:
[MCU2_0] 832.018317 s: Driver create failed!!
[MCU2_0] 832.018352 s: VX_ZONE_ERROR:[tivxCaptureCreate:1206] : Capture Create Failed!!!
Thanks
Regards
Shine