Other Parts Discussed in Thread: TPS65219, SN74LVC244A
Hello TI
I am reviewing the design file (SPRR453.ZIP) for the SK-AM62-P1 EVM with TPS65219 PMIC.
The BOOT MODE SWITCHES (SW1, SW2) are currently pulled up to VCC3V3_TA.
The BOOT MODE BUFFERS (U73, U75) use SN74AVC8T245RHL to perform voltage level translation between VCC3V3_TA (VCCA) and VCC_3V3_SYS (VCCB).
Please provide information on the following:
(1) Is it possible to change the pull-up of BOOT MODE SWITCHES (SW1, SW2) to VCC_3V3_SYS?
(2) Could you explain the reason for using SN74AVC8T245RHL in the BOOT MODE BUFFERS (U73, U75)?
Additionally, is it feasible to use SN74LVC244A with VCC=VCC_3V3_SYS in the BOOT MODE BUFFERS?
Regards,
user3895290