Hi All,
I am using cortex-A8 AEC on omap-4 platform. anyone has done this AEC on Omap4 (pandaboard) platform and can it be done as alsa plugin?
Regards,
Ashwani
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Aswani,
We will be using this in Android on OMAP4 (tablet, but will also be released to pandaboard) where it will stack above ALSA in the Audio HAL layer.
Thanks and Regards,
Samant
We are using ubuntu 10.10 on omap4 platform. If you already done AEC on omap4(pandaboard) can you share it?
AER Cortex-A8 obj 15_1_10_3 Linux .
downloaded from:
http://software-dl.ti.com/sdoemb/sdoemb_registered_sw/aer/15_1_10_3/index_FDS.html
got reference from http://e2e.ti.com/support/embedded/f/356/t/109612.aspx .
For creating AER alsa plug-in, we need AER shared libraries (dynamic) but we have static libraries(aer_a.av7A, aer_c.av7A) available from the cortex-A8 AER. We are facing issues like "Linking the shared library against the static library is not portable! " while building the AER alsa plug-in.
Can TI provide the AER dynamic libraries(.so)?
Hi Ashwani,
Since, the AER is a very low level signal processing component there is no plan for release of a shared library. But we are planning/working on a higher level component which will include AER and other components for Linux/Android and that *may* be in a shared library form.
Though you can wrap existing AER component in a shared library. Try this out http://stackoverflow.com/questions/1614970/c-linker-question-dynamic-and-static-library-dependency.
Hope it helps.
Thanks,