Hi,
I would like to change the USB polling interval. My kernel version is 4.9.31. When i verify the code, polling interval is being configured based on USB speed.
Below is the information that I need:
a) Configurable option for setting USB polling interval. If it is not possible, where could I directly hard code in the USB driver?
b) Could you also help understand what should be an optimal value for the polling interval? What are the consequences of increasing/decreasing this value?
Thanks,
Naresh