This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6000-CGT: Software Downloads

Part Number: C6000-CGT

Hello Team,

As a part of Confidence From Use to Fill TQP and TQR i need  the below information:

I am using ti_cgt_c6000_8.3.7.

  • user statistics has been obtained from Texas instruments. It shows that many users are using this version of the compiler

Also the .xls sheet for the known bug Analyses and Workarounds. I didnt find  workarounds bugs everything in single page.

Thanks

Poornima

  • Regarding downloads of ti_cgt_c6000_8.3.7, I have attached a file below.  It is a CSV file you can open with a spreadsheet program like Excel.  Remove the file extension .txt before working with it.

    Regarding ...

    the .xls sheet for the known bug Analyses and Workarounds

    the template file TQM.docm contains the following:


    1.1      Known Bug Analysis (Example)

    The following issues have been received from Texas Instruments on November 11th and classified to have impact (see relevant_issues.xls for more details and the mapping to the mitigations)

    1. CODEGEN-6469
    2. CODEGEN-6070

     

    The following work arounds are required for the known issues:

    1. use work around in:

    e2e.ti.com/.../3026599 or avoid exceptions/C++

    1. avoid duplicated type definitions

    The work arounds have been added to the tool safety manual


    All of this is an example.  You are expected to completely rewrite it.  With regard to the file relevant_issues.xls, you are expected to supply it.  The best place to start is the file README.html in the root directory of the compiler installation.  It contains a list of resolved and known defects.

    Thanks and regards,

    -George

    Software File Name	2022	2023	Grand total
    TI_CGT_C6000_8.3.7_LINUX_INSTALLER_X86.BIN	16	13	29
    TI_CGT_C6000_8.3.7_OSX_INSTALLER.APP.ZIP	3		3
    TI_CGT_C6000_8.3.7_WINDOWS_INSTALLER.EXE	14	3	17