Other Parts Discussed in Thread: TPIC2810
i am trying to access the gpio pins through terminal itself. i am using gpio tools like gpiodetect and gpioinfo to access the pins but gpiochip 2 and 3 all that showing unnamed, or we can say not labeled so i am not able to access the gpio pins. I request you to help me with the same. Below is the terminal output for gpioinfo :
gpiochip2 - 87 lines:
line 0: unnamed unused input active-high
line 1: unnamed unused input active-high
line 2: unnamed unused input active-high
I am not able to access these pins and I don't have knowledge of which pin is connect to which header.
In gpiochip1, the pins are labeled so i'm able to access them.
gpiochip1 - 8 lines:
line 0: "GPIO_CPSW2_RST" unused input active-high
line 1: "GPIO_CPSW1_RST" unused input active-high
line 2: "PRU_DETECT" unused input active-high
line 3: "MMC1_SD_EN" "fixed-regulator-sd" output active-high [used]
line 4: "VPP_LDO_EN" unused input active-high
line 5: "RPI_PS_3V3_En" unused input active-high
line 6: "RPI_PS_5V0_En" unused input active-high
line 7: "RPI_HAT_DETECT" unused input active-high