Part Number: LP-AM263
I am using LP-AM263 and I want to know how can I trace the CPU and memory utilization step by step in my program
Have any idea or tools I can use?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-AM263
I am using LP-AM263 and I want to know how can I trace the CPU and memory utilization step by step in my program
Have any idea or tools I can use?
Hi Charlie,
CPU Load trace:
The below code snippet will be useful to calculate CPU load for your program. You can change the time interval (default I've shared is for 5 seconds, i.e., CPU load will be printed every 5 seconds). The CPU load is calculated with respect to the time IDLE task was running.
#include "FreeRTOS.h"
#include "task.h"
#include <kernel/dpl/TaskP.h>
#include <kernel/dpl/ClockP.h>
TaskStatus_t gTaskStatusArr[32] ={0};
uint32_t gNumTask = 0U;
void print_cpu_load()
{
static uint32_t start_time = 0;
uint32_t print_interval_in_secs = 5;
uint32_t cur_time = ClockP_getTimeUsec()/1000;
uint32_t totalRunTime = 0U;
if(start_time==0)
{
start_time = cur_time;
}
else
if( (cur_time-start_time) >= (print_interval_in_secs*1000) )
{
uint32_t cpu_load = TaskP_loadGetTotalCpuLoad();
DebugP_log(" %6d.%3ds : CPU load = %3d.%02d %%\r\n",
cur_time/1000, cur_time%1000,
cpu_load/100, cpu_load%100 );
start_time = cur_time;
gNumTask = uxTaskGetSystemState(&gTaskStatusArr[0], 32U, &totalRunTime);
TaskP_loadResetAll();
}
}
Memory Trace:
To get the memory usage statistics of heap, you can use APIs provided by FreeRTOS DPL (HeapP.c)
Make sure to include the FreeRTOS library and the required HeapP files, then call
void HeapP_getHeapStats( HeapP_Object *heap, HeapP_MemStats * pHeapStats )
Regards,
Shaunak