This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: U-Boot SPI issues with SDK V9

Part Number: TMDS64EVM

Hi,

Since I migrated my yocto project from V8.6 to V9 I haven't been able to use the integrated SPI NOR on the EVM in U-Boot.

> sf probe                                                        
ti_sci system-controller@44043000: Message not acknowledgedti-sci-pm-domains po)
Invalid bus 0 (err=-19)                                                         
Failed to initialize SPI flash at 0:0 (error 0)

I'm using the latest SDK V09.00.00.009 but observed the issue across all version since V9. The image I'm compiling is tisdk-base-image.bb

Any clue ?

Regards
Pierre