This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Target kernel, TIVX_CMD_NODE_CREATE failed for node PreProcNode

Part Number: TDA4VM

Hello Team,

I have two different applications successfully running on 08_05_00_11 migrated to 08_06_01_03 and working fine, please find the applications below.

1)Taken app_tidl_od_cam application and made changes as per requirement. This application performs color conversion and 4-output mosaic image.

2)Taken app_tidl_od and integrated custom post proc kernel in which draw detections too included, detects objects of different classes.

Both these are working fine individually in both the SDK versions.

Now I'm integrating the 2nd application into the 1st application on SDK v 08_06_01_03. I have integrated each module from 2nd application to 1st application and made the necessary changes.There are no build errors, but getting few run time errors.

Please find the attached file for the run time log and ignore the debug statements.

j7-evm login: root
root@j7-evm:~# cd /opt/vision_apps/
root@j7-evm:/opt/vision_apps# source ./vision_apps_init.sh 
root@j7-evm:/opt/vision_apps# [MCU2_0]      4.205280 s: CIO: Init ... Done !!!
[MCU2_0]      4.205349 s: ### CPU Frequency = 1000000000 Hz
[MCU2_0]      4.205389 s: CPU is running FreeRTOS
[MCU2_0]      4.205415 s: APP: Init ... !!!
[MCU2_0]      4.205440 s: SCICLIENT: Init ... !!!
[MCU2_0]      4.205732 s: SCICLIENT: DMSC FW version [8.6.3--v08.06.03 (Chill Capybar]
[MCU2_0]      4.205781 s: SCICLIENT: DMSC FW revision 0x8  
[MCU2_0]      4.205816 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_0]      4.205853 s: SCICLIENT: Init ... Done !!!
[MCU2_0]      4.205881 s: UDMA: Init ... !!!
[MCU2_0]      4.207301 s: UDMA: Init ... Done !!!
[MCU2_0]      4.207366 s: MEM: Init ... !!!
[MCU2_0]      4.207411 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ d9000000 of size 16777216 bytes !!!
[MCU2_0]      4.207488 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!!
[MCU2_0]      4.207549 s: MEM: Init ... Done !!!
[MCU2_0]      4.207574 s: IPC: Init ... !!!
[MCU2_0]      4.207636 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_0]      4.207685 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_0]     16.417292 s: IPC: HLOS is ready !!!
[MCU2_0]     16.432634 s: IPC: Init ... Done !!!
[MCU2_0]     16.432701 s: APP: Syncing with 5 CPUs ... !!!
[MCU2_0]     16.589653 s: APP: Syncing with 5 CPUs ... Done !!!
[MCU2_0]     16.589878 s: REMOTE_SERVICE: Init ... !!!
[MCU2_0]     16.591565 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_0]     16.591625 s: ETHFW: Init ... !!!
[MCU2_0]     16.596536 s: Warning: Using 6 MAC address(es) from static pool
[MCU2_0]     16.596652 s: ETHFW: Shared multicasts (software fanout):
[MCU2_0]     16.596696 s: ETHFW: Reserved multicasts:
[MCU2_0]     16.596725 s:   01:80:c2:00:00:0e
[MCU2_0]     16.596776 s:   01:1b:19:00:00:00
[MCU2_0]     16.597039 s: EnetMcm: CPSW_9G on MAIN NAVSS
[MCU2_0]     16.606436 s: Mdio_open: MDIO manual mode enabled
[MCU2_0]     16.610386 s: PHY 16 is alive
[MCU2_0]     16.610540 s: PHY 17 is alive
[MCU2_0]     16.610651 s: PHY 18 is alive
[MCU2_0]     16.610756 s: PHY 19 is alive
[MCU2_0]     16.613963 s: 
[MCU2_0] ETHFW Version   : 0.02.00
[MCU2_0]     16.614049 s: ETHFW Build Date: Sep  8, 2023
[MCU2_0]     16.614082 s: ETHFW Build Time: 17:08:52
[MCU2_0]     16.614112 s: ETHFW Commit SHA: 
[MCU2_0]     16.614186 s: ETHFW: Init ... DONE !!!
[MCU2_0]     16.614220 s: ETHFW: Remove server Init ... !!!
[MCU2_0]     16.614397 s: CpswProxyServer: Virtual port configuration:
[MCU2_0]     16.614455 s:   mpu_1_0 <-> Switch port 0: mpu_1_0_ethswitch-device-0
[MCU2_0]     16.614501 s:   mcu_2_1 <-> Switch port 1: mcu_2_1_ethswitch-device-1
[MCU2_0]     16.614544 s:   mpu_1_0 <-> MAC port 1: mpu_1_0_ethmac-device-1
[MCU2_0]     16.614585 s:   mcu_2_1 <-> MAC port 4: mcu_2_1_ethmac-device-4
[MCU2_0]     16.615613 s: CpswProxyServer: initialization completed (core: mcu2_0)
[MCU2_0]     16.615682 s: ETHFW: Remove server Init ... DONE !!!
[MCU2_0]     16.616836 s: Starting lwIP, local interface IP is dhcp-enabled
[MCU2_0]     16.625099 s: Host MAC address: 70:ff:76:1d:92:c3
[MCU2_0]     16.629320 s: [LWIPIF_LWIP] Enet LLD netif initialized successfully
[MCU2_0]     16.629415 s: Added interface 'ti1', IP is 0.0.0.0
[MCU2_0]     16.665000 s: FVID2: Init ... !!!
[MCU2_0]     16.665114 s: FVID2: Init ... Done !!!
[MCU2_0]     16.665169 s: DSS: Init ... !!!
[MCU2_0]     16.665199 s: DSS: Display type is eDP !!!
[MCU2_0]     16.665230 s: DSS: M2M Path is enabled !!!
[MCU2_0]     16.665259 s: DSS: SoC init ... !!!
[MCU2_0]     16.665284 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2
[MCU2_0]     16.665505 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.665546 s: SCICLIENT: Sciclient_pmSetModuleState module=297 state=2
[MCU2_0]     16.665739 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.665776 s: SCICLIENT: Sciclient_pmSetModuleState module=151 state=2
[MCU2_0]     16.665939 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.666082 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=9 parent=11
[MCU2_0]     16.666241 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]     16.666281 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=13 parent=18
[MCU2_0]     16.666403 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]     16.666443 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=1 parent=2
[MCU2_0]     16.666554 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]     16.666590 s: SCICLIENT: Sciclient_pmSetModuleClkFreq module=152 clk=1 freq=148500000
[MCU2_0]     16.667811 s: SCICLIENT: Sciclient_pmSetModuleClkFreq success
[MCU2_0]     16.667863 s: SCICLIENT: Sciclient_pmModuleClkRequest module=152 clk=1 state=2 flag=0
[MCU2_0]     16.668048 s: SCICLIENT: Sciclient_pmModuleClkRequest success
[MCU2_0]     16.668098 s: DSS: SoC init ... Done !!!
[MCU2_0]     16.668130 s: DSS: Board init ... !!!
[MCU2_0]     16.668156 s: DSS: Board init ... Done !!!
[MCU2_0]     16.704913 s: DSS: Init ... Done !!!
[MCU2_0]     16.705099 s: VHWA: VPAC Init ... !!!
[MCU2_0]     16.705146 s: SCICLIENT: Sciclient_pmSetModuleState module=290 state=2
[MCU2_0]     16.705360 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.705402 s: VHWA: LDC Init ... !!!
[MCU2_0]     16.709114 s: VHWA: LDC Init ... Done !!!
[MCU2_0]     16.709183 s: VHWA: MSC Init ... !!!
[MCU2_0]     16.721541 s: VHWA: MSC Init ... Done !!!
[MCU2_0]     16.721610 s: VHWA: NF Init ... !!!
[MCU2_0]     16.723551 s: VHWA: NF Init ... Done !!!
[MCU2_0]     16.723617 s: VHWA: VISS Init ... !!!
[MCU2_0]     16.735314 s: VHWA: VISS Init ... Done !!!
[MCU2_0]     16.735380 s: VHWA: VPAC Init ... Done !!!
[MCU2_0]     16.735427 s:  VX_ZONE_INIT:Enabled
[MCU2_0]     16.735460 s:  VX_ZONE_ERROR:Enabled
[MCU2_0]     16.735490 s:  VX_ZONE_WARNING:Enabled
[MCU2_0]     16.737133 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target MCU2-0 
[MCU2_0]     16.737468 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_NF 
[MCU2_0]     16.737761 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_LDC1 
[MCU2_0]     16.738188 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC1 
[MCU2_0]     16.738470 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC2 
[MCU2_0]     16.738761 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_VISS1 
[MCU2_0]     16.739152 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE1 
[MCU2_0]     16.739456 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE2 
[MCU2_0]     16.739742 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DISPLAY1 
[MCU2_0]     16.740143 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DISPLAY2 
[MCU2_0]     16.740425 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CSITX 
[MCU2_0]     16.740717 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE3 
[MCU2_0]     16.741115 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE4 
[MCU2_0]     16.741433 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE5 
[MCU2_0]     16.741732 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE6 
[MCU2_0]     16.742133 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE7 
[MCU2_0]     16.742447 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE8 
[MCU2_0]     16.742716 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M1 
[MCU2_0]     16.743110 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M2 
[MCU2_0]     16.743415 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M3 
[MCU2_0]     16.743676 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M4 
[MCU2_0]     16.743736 s:  VX_ZONE_INIT:[tivxInitLocal:148] Initialization Done !!!
[MCU2_0]     16.743772 s: APP: OpenVX Target kernel init ... !!!
[MCU2_0]     16.767834 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_0]     16.767905 s: CSI2RX: Init ... !!!
[MCU2_0]     16.767934 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_0]     16.768206 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.768261 s: SCICLIENT: Sciclient_pmSetModuleState module=26 state=2
[MCU2_0]     16.768426 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.768465 s: SCICLIENT: Sciclient_pmSetModuleState module=27 state=2
[MCU2_0]     16.768672 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.768706 s: SCICLIENT: Sciclient_pmSetModuleState module=147 state=2
[MCU2_0]     16.768809 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.768843 s: SCICLIENT: Sciclient_pmSetModuleState module=148 state=2
[MCU2_0]     16.769067 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.769323 s: CSI2RX: Init ... Done !!!
[MCU2_0]     16.769364 s: CSI2TX: Init ... !!!
[MCU2_0]     16.769392 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_0]     16.769503 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.769543 s: SCICLIENT: Sciclient_pmSetModuleState module=28 state=2
[MCU2_0]     16.769686 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.769721 s: SCICLIENT: Sciclient_pmSetModuleState module=296 state=2
[MCU2_0]     16.769839 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     16.769914 s: CSI2TX: Init ... Done !!!
[MCU2_0]     16.769951 s: ISS: Init ... !!!
[MCU2_0]     16.770094 s: Found sensor IMX390-UB953_D3 at location 0 
[MCU2_0]     16.770160 s: Found sensor AR0233-UB953_MARS at location 1 
[MCU2_0]     16.770203 s: Found sensor AR0820-UB953_LI at location 2 
[MCU2_0]     16.770241 s: Found sensor UB9xxx_RAW12_TESTPATTERN at location 3 
[MCU2_0]     16.770282 s: Found sensor UB96x_UYVY_TESTPATTERN at location 4 
[MCU2_0]     16.770321 s: Found sensor GW_AR0233_UYVY at location 5 
[MCU2_0]     16.770358 s: Found sensor ISX016-UB913 at location 6 
[MCU2_0]     16.770404 s: IssSensor_ISX016_Init Success
[MCU2_0]     16.770435 s: IssSensor_Init ... Done !!!
[MCU2_0]     16.770524 s: IttRemoteServer_Init ... Done !!!
[MCU2_0]     16.770562 s: VISS REMOTE SERVICE: Init ... !!!
[MCU2_0]     16.770628 s: VISS REMOTE SERVICE: Init ... Done !!!
[MCU2_0]     16.770663 s: UDMA Copy: Init ... !!!
[MCU2_0]     16.772609 s: UDMA Copy: Init ... Done !!!
[MCU2_0]     16.772717 s: APP: Init ... Done !!!
[MCU2_0]     16.772758 s: APP: Run ... !!!
[MCU2_0]     16.772784 s: IPC: Starting echo test ...
[MCU2_0]     16.776111 s: APP: Run ... Done !!!
[MCU2_0]     16.777721 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C66X_1[P] C66X_2[.] C7X_1[.] 
[MCU2_0]     16.777887 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C66X_1[P] C66X_2[P] C7X_1[.] 
[MCU2_0]     16.778136 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[.] 
[MCU2_0]     16.778246 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[P] 
[MCU2_0]     16.854356 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6
[MCU2_0]     17.215060 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6
[MCU2_0]     19.663338 s: Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c2, FlowIdx:173, FlowIdxOffset:1
[MCU2_0]     19.699376 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6,mode:disable
[MCU2_0]     19.701087 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6,mode:disable
[MCU2_0]     19.701589 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6,mode:disable
[MCU2_0]     19.716310 s: Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c1, FlowIdx:172, FlowIdxOffset:0
[MCU2_0]     19.719503 s: Cpsw_ioctlInternal: CPSW: Registered MAC address. ALE entry:11, Policer Entry:2
[MCU2_0]     19.753625 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:33:33:0:0:0:1, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     19.757152 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:1:0:5e:0:0:1, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     19.760611 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:33:33:ff:1d:92:c1, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     19.838573 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6,mode:disable
[MCU2_0]     19.838862 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6,mode:disable
[MCU2_0]     19.859481 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:0, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     19.869609 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:3, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     19.873151 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:e, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     19.873312 s: CpswProxyServer_isRsvdMcast: Reserved mcast cannot be added to filter
[MCU2_0]     19.985838 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6,mode:disable
[MCU2_0]     19.986210 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:33:33:0:0:0:fb, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     21.689218 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6, MacAddress:33:33:0:1:0:3, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]     21.721119 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a3ac8184,CoreKey:38acb7e6,mode:disable
[MCU2_1]      4.150806 s: CIO: Init ... Done !!!
[MCU2_1]      4.150877 s: ### CPU Frequency = 1000000000 Hz
[MCU2_1]      4.150917 s: CPU is running FreeRTOS
[MCU2_1]      4.150943 s: APP: Init ... !!!
[MCU2_1]      4.150965 s: SCICLIENT: Init ... !!!
[MCU2_1]      4.151226 s: SCICLIENT: DMSC FW version [8.6.3--v08.06.03 (Chill Capybar]
[MCU2_1]      4.151276 s: SCICLIENT: DMSC FW revision 0x8  
[MCU2_1]      4.151309 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_1]      4.151364 s: SCICLIENT: Init ... Done !!!
[MCU2_1]      4.151392 s: UDMA: Init ... !!!
[MCU2_1]      4.152818 s: UDMA: Init ... Done !!!
[MCU2_1]      4.152877 s: MEM: Init ... !!!
[MCU2_1]      4.152917 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ da000000 of size 16777216 bytes !!!
[MCU2_1]      4.152991 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 3640000 of size 262144 bytes !!!
[MCU2_1]      4.153052 s: MEM: Init ... Done !!!
[MCU2_1]      4.153078 s: IPC: Init ... !!!
[MCU2_1]      4.153141 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_1]      4.153191 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_1]     16.574292 s: IPC: HLOS is ready !!!
[MCU2_1]     16.589535 s: IPC: Init ... Done !!!
[MCU2_1]     16.589602 s: APP: Syncing with 5 CPUs ... !!!
[MCU2_1]     16.589651 s: APP: Syncing with 5 CPUs ... Done !!!
[MCU2_1]     16.589688 s: REMOTE_SERVICE: Init ... !!!
[MCU2_1]     16.591425 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_1]     16.591490 s: FVID2: Init ... !!!
[MCU2_1]     16.591560 s: FVID2: Init ... Done !!!
[MCU2_1]     16.591596 s: VHWA: DMPAC: Init ... !!!
[MCU2_1]     16.591622 s: SCICLIENT: Sciclient_pmSetModuleState module=48 state=2
[MCU2_1]     16.592160 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1]     16.592202 s: SCICLIENT: Sciclient_pmSetModuleState module=305 state=2
[MCU2_1]     16.592658 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1]     16.592696 s: VHWA: DOF Init ... !!!
[MCU2_1]     16.600999 s: VHWA: DOF Init ... Done !!!
[MCU2_1]     16.601066 s: VHWA: SDE Init ... !!!
[MCU2_1]     16.603721 s: VHWA: SDE Init ... Done !!!
[MCU2_1]     16.603781 s: VHWA: DMPAC: Init ... Done !!!
[MCU2_1]     16.603827 s:  VX_ZONE_INIT:Enabled
[MCU2_1]     16.603858 s:  VX_ZONE_ERROR:Enabled
[MCU2_1]     16.603885 s:  VX_ZONE_WARNING:Enabled
[MCU2_1]     16.605300 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target MCU2-1 
[MCU2_1]     16.605564 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DMPAC_SDE 
[MCU2_1]     16.605786 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DMPAC_DOF 
[MCU2_1]     16.605843 s:  VX_ZONE_INIT:[tivxInitLocal:148] Initialization Done !!!
[MCU2_1]     16.605880 s: APP: OpenVX Target kernel init ... !!!
[MCU2_1]     16.606155 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_1]     16.606192 s: UDMA Copy: Init ... !!!
[MCU2_1]     16.608184 s: UDMA Copy: Init ... Done !!!
[MCU2_1]     16.608258 s: APP: Init ... Done !!!
[MCU2_1]     16.608290 s: APP: Run ... !!!
[MCU2_1]     16.608327 s: IPC: Starting echo test ...
[MCU2_1]     16.610884 s: APP: Run ... Done !!!
[MCU2_1]     16.612016 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[.] C7X_1[.] 
[MCU2_1]     16.612129 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[.] 
[MCU2_1]     16.612223 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[P] 
[MCU2_1]     16.776887 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[P] 
[C6x_1 ]      4.205684 s: CIO: Init ... Done !!!
[C6x_1 ]      4.205712 s: ### CPU Frequency = 1350000000 Hz
[C6x_1 ]      4.205722 s: CPU is running FreeRTOS
[C6x_1 ]      4.205730 s: APP: Init ... !!!
[C6x_1 ]      4.205738 s: SCICLIENT: Init ... !!!
[C6x_1 ]      4.205934 s: SCICLIENT: DMSC FW version [8.6.3--v08.06.03 (Chill Capybar]
[C6x_1 ]      4.205946 s: SCICLIENT: DMSC FW revision 0x8  
[C6x_1 ]      4.205956 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_1 ]      4.205966 s: SCICLIENT: Init ... Done !!!
[C6x_1 ]      4.205975 s: UDMA: Init ... !!!
[C6x_1 ]      4.207848 s: UDMA: Init ... Done !!!
[C6x_1 ]      4.207865 s: MEM: Init ... !!!
[C6x_1 ]      4.207877 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ dc000000 of size 16777216 bytes !!!
[C6x_1 ]      4.207894 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_1 ]      4.207910 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ dd000000 of size 50331648 bytes !!!
[C6x_1 ]      4.207926 s: MEM: Init ... Done !!!
[C6x_1 ]      4.207934 s: IPC: Init ... !!!
[C6x_1 ]      4.207953 s: IPC: 6 CPUs participating in IPC !!!
[C6x_1 ]      4.207965 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_1 ]     15.838267 s: IPC: HLOS is ready !!!
[C6x_1 ]     15.842322 s: IPC: Init ... Done !!!
[C6x_1 ]     15.842349 s: APP: Syncing with 5 CPUs ... !!!
[C6x_1 ]     16.589650 s: APP: Syncing with 5 CPUs ... Done !!!
[C6x_1 ]     16.589664 s: REMOTE_SERVICE: Init ... !!!
[C6x_1 ]     16.590302 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_1 ]     16.590336 s:  VX_ZONE_INIT:Enabled
[C6x_1 ]     16.590347 s:  VX_ZONE_ERROR:Enabled
[C6x_1 ]     16.590356 s:  VX_ZONE_WARNING:Enabled
[C6x_1 ]     16.591157 s:  VX_ZONE_INIT:[tivxInitLocal:148] Initialization Done !!!
[C6x_1 ]     16.591170 s: APP: OpenVX Target kernel init ... !!!
[C6x_1 ]     16.591331 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_1 ]     16.591347 s: UDMA Copy: Init ... !!!
[C6x_1 ]     16.595026 s: UDMA Copy: Init ... Done !!!
[C6x_1 ]     16.595046 s: APP: Init ... Done !!!
[C6x_1 ]     16.595055 s: APP: Run ... !!!
[C6x_1 ]     16.595063 s: IPC: Starting echo test ...
[C6x_1 ]     16.596131 s: APP: Run ... Done !!!
[C6x_1 ]     16.596428 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[s] C66X_2[x] C7X_1[P] 
[C6x_1 ]     16.596758 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[s] C66X_2[P] C7X_1[P] 
[C6x_1 ]     16.611425 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[s] C66X_2[P] C7X_1[P] 
[C6x_1 ]     16.776746 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[s] C66X_2[P] C7X_1[P] 
[C6x_2 ]      4.283872 s: CIO: Init ... Done !!!
[C6x_2 ]      4.283900 s: ### CPU Frequency = 1350000000 Hz
[C6x_2 ]      4.283910 s: CPU is running FreeRTOS
[C6x_2 ]      4.283919 s: APP: Init ... !!!
[C6x_2 ]      4.283927 s: SCICLIENT: Init ... !!!
[C6x_2 ]      4.284132 s: SCICLIENT: DMSC FW version [8.6.3--v08.06.03 (Chill Capybar]
[C6x_2 ]      4.284145 s: SCICLIENT: DMSC FW revision 0x8  
[C6x_2 ]      4.284155 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_2 ]      4.284165 s: SCICLIENT: Init ... Done !!!
[C6x_2 ]      4.284175 s: UDMA: Init ... !!!
[C6x_2 ]      4.285677 s: UDMA: Init ... Done !!!
[C6x_2 ]      4.285695 s: MEM: Init ... !!!
[C6x_2 ]      4.285707 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ e0000000 of size 16777216 bytes !!!
[C6x_2 ]      4.285725 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_2 ]      4.285741 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ e1000000 of size 50331648 bytes !!!
[C6x_2 ]      4.285757 s: MEM: Init ... Done !!!
[C6x_2 ]      4.285765 s: IPC: Init ... !!!
[C6x_2 ]      4.285785 s: IPC: 6 CPUs participating in IPC !!!
[C6x_2 ]      4.285798 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_2 ]     15.945742 s: IPC: HLOS is ready !!!
[C6x_2 ]     15.949427 s: IPC: Init ... Done !!!
[C6x_2 ]     15.949454 s: APP: Syncing with 5 CPUs ... !!!
[C6x_2 ]     16.589651 s: APP: Syncing with 5 CPUs ... Done !!!
[C6x_2 ]     16.589664 s: REMOTE_SERVICE: Init ... !!!
[C6x_2 ]     16.590313 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_2 ]     16.590345 s:  VX_ZONE_INIT:Enabled
[C6x_2 ]     16.590355 s:  VX_ZONE_ERROR:Enabled
[C6x_2 ]     16.590365 s:  VX_ZONE_WARNING:Enabled
[C6x_2 ]     16.591162 s:  VX_ZONE_INIT:[tivxInitLocal:148] Initialization Done !!!
[C6x_2 ]     16.591176 s: APP: OpenVX Target kernel init ... !!!
[C6x_2 ]     16.591340 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_2 ]     16.591356 s: UDMA Copy: Init ... !!!
[C6x_2 ]     16.595221 s: UDMA Copy: Init ... Done !!!
[C6x_2 ]     16.595245 s: APP: Init ... Done !!!
[C6x_2 ]     16.595254 s: APP: Run ... !!!
[C6x_2 ]     16.595263 s: IPC: Starting echo test ...
[C6x_2 ]     16.596415 s: APP: Run ... Done !!!
[C6x_2 ]     16.596687 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[.] 
[C6x_2 ]     16.596765 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[P] 
[C6x_2 ]     16.611452 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[P] C66X_2[s] C7X_1[P] 
[C6x_2 ]     16.776793 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[P] C66X_2[s] C7X_1[P] 
[C7x_1 ]      4.509837 s: CIO: Init ... Done !!!
[C7x_1 ]      4.509852 s: ### CPU Frequency = 1000000000 Hz
[C7x_1 ]      4.509863 s: CPU is running FreeRTOS
[C7x_1 ]      4.509871 s: APP: Init ... !!!
[C7x_1 ]      4.509878 s: SCICLIENT: Init ... !!!
[C7x_1 ]      4.510084 s: SCICLIENT: DMSC FW version [8.6.3--v08.06.03 (Chill Capybar]
[C7x_1 ]      4.510099 s: SCICLIENT: DMSC FW revision 0x8  
[C7x_1 ]      4.510109 s: SCICLIENT: DMSC FW ABI revision 3.1
[C7x_1 ]      4.510120 s: SCICLIENT: Init ... Done !!!
[C7x_1 ]      4.510129 s: UDMA: Init ... !!!
[C7x_1 ]      4.511251 s: UDMA: Init ... Done !!!
[C7x_1 ]      4.511263 s: MEM: Init ... !!!
[C7x_1 ]      4.511275 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ 117000000 of size 268435456 bytes !!!
[C7x_1 ]      4.511296 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 70020000 of size 8159232 bytes !!!
[C7x_1 ]      4.511314 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 64800000 of size 458752 bytes !!!
[C7x_1 ]      4.511331 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 64e00000 of size 16384 bytes !!!
[C7x_1 ]      4.511348 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ 100000000 of size 385875968 bytes !!!
[C7x_1 ]      4.511366 s: MEM: Init ... Done !!!
[C7x_1 ]      4.511374 s: IPC: Init ... !!!
[C7x_1 ]      4.511388 s: IPC: 6 CPUs participating in IPC !!!
[C7x_1 ]      4.511402 s: IPC: Waiting for HLOS to be ready ... !!!
[C7x_1 ]     16.128266 s: IPC: HLOS is ready !!!
[C7x_1 ]     16.130323 s: IPC: Init ... Done !!!
[C7x_1 ]     16.130337 s: APP: Syncing with 5 CPUs ... !!!
[C7x_1 ]     16.589652 s: APP: Syncing with 5 CPUs ... Done !!!
[C7x_1 ]     16.589670 s: REMOTE_SERVICE: Init ... !!!
[C7x_1 ]     16.589819 s: REMOTE_SERVICE: Init ... Done !!!
[C7x_1 ]     16.589840 s:  VX_ZONE_INIT:Enabled
[C7x_1 ]     16.589850 s:  VX_ZONE_ERROR:Enabled
[C7x_1 ]     16.589860 s:  VX_ZONE_WARNING:Enabled
[C7x_1 ]     16.590014 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1 
[C7x_1 ]     16.590111 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2 
[C7x_1 ]     16.590198 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3 
[C7x_1 ]     16.590268 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4 
[C7x_1 ]     16.590330 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5 
[C7x_1 ]     16.590407 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6 
[C7x_1 ]     16.590517 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7 
[C7x_1 ]     16.590581 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8 
[C7x_1 ]     16.590602 s:  VX_ZONE_INIT:[tivxInitLocal:148] Initialization Done !!!
[C7x_1 ]     16.590614 s: APP: OpenVX Target kernel init ... !!!
[C7x_1 ]     16.590763 s: APP: OpenVX Target kernel init ... Done !!!
[C7x_1 ]     16.590776 s: APP: Init ... Done !!!
[C7x_1 ]     16.590786 s: APP: Run ... !!!
[C7x_1 ]     16.590794 s: IPC: Starting echo test ...
[C7x_1 ]     16.590953 s: APP: Run ... Done !!!
[C7x_1 ]     16.596435 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[x] C7X_1[s] 
[C7x_1 ]     16.596762 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[P] C7X_1[s] 
[C7x_1 ]     16.611474 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[s] 
[C7x_1 ]     16.776824 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[s] 

root@j7-evm:/opt/vision_apps# ./run_rci_tidl_od_cam.sh 
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
    41.331986 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
    41.337752 s:  VX_ZONE_INIT:Enabled
    41.337783 s:  VX_ZONE_ERROR:Enabled
    41.337789 s:  VX_ZONE_WARNING:Enabled
    41.338789 s:  VX_ZONE_INIT:[tivxInitLocal:148] Initialization Done !!!
    41.339895 s:  VX_ZONE_INIT:[tivxHostInitLocal:93] Initialization Done for HOST !!!
before app_default_param_set 
after app_default_param_set 
Default param set! 
before  app_parse_cmd_line_args 
after app_parse_cmd_line_args  
Parsed user params! 
before app_querry_sensor  
    41.344247 s: ISS: Enumerating sensors ... !!!
[MCU2_0]     41.344493 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_ENUMERATE 
[MCU2_0]     41.344770 s: write 0xfe to TCA6408 register 0x3 
[MCU2_0]     41.444002 s: RE-SETTING FUSION2 DE-SER !!!!!!
[MCU2_0]     41.444068 s: UB960 config start 
[MCU2_0]     44.004289 s: End of UB960 config 
[MCU2_0]     44.004355 s: UB960 config start 
    44.430529 s: ISS: Enumerating sensors ... found 0 : IMX390-UB953_D3
    44.430575 s: ISS: Enumerating sensors ... found 1 : AR0233-UB953_MARS
    44.430581 s: ISS: Enumerating sensors ... found 2 : AR0820-UB953_LI
    44.430587 s: ISS: Enumerating sensors ... found 3 : UB9xxx_RAW12_TESTPATTERN
    44.430592 s: ISS: Enumerating sensors ... found 4 : UB96x_UYVY_TESTPATTERN
    44.430597 s: ISS: Enumerating sensors ... found 5 : GW_AR0233_UYVY
    44.430602 s: ISS: Enumerating sensors ... found 6 : ISX016-UB913
Sensor index : 6
Sensor selected : ISX016-UB913
Querying ISX016-UB913 
    44.430622 s: ISS: Querying sensor [ISX016-UB913] ... !!!
    44.431095 s: ISS: Querying sensor [ISX016-UB913] ... Done !!!
Sensor pixel container is UYVY 
Sensor mask : 15 
 Total num of cameras enabled : 4 
after app_querry_sensor  
Sensor params queried! 
before  app_update_param_set 
 ### APP DEBUG: width = 1280, height = 724after app_update_param_set  
Updated user params! 
before  app_init 
Creating context done!
[MCU2_0]     44.430280 s: End of UB960 config 
[MCU2_0]     44.430813 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_QUERY 
[MCU2_0]     44.430875 s: Received Query for ISX016-UB913 
entered tivxAddTargetKernelRciPostprocA72
exit tivxAddTargetKernelRciPostprocA72
before tivxColorConvKernelLoadKernels
after tivxColorConvKernelLoadKernels
Kernel loading done!
    44.445231 s: ISS: Initializing sensor [ISX016-UB913], doing IM_SENSOR_CMD_PWRON ... !!!
    44.445846 s: ISS: Initializing sensor [ISX016-UB913], doing IM_SENSOR_CMD_CONFIG ... !!!
[MCU2_0]     44.445422 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_PWRON 
[MCU2_0]     44.445489 s: IM_SENSOR_CMD_PWRON : channel_mask = 0xf 
[MCU2_0]     44.445562 s: ISX016_PowerOn : chId = 0x0 
[MCU2_0]     44.445606 s: ISX016_PowerOn : chId = 0x1 
[MCU2_0]     44.445644 s: ISX016_PowerOn : chId = 0x2 
[MCU2_0]     44.445680 s: ISX016_PowerOn : chId = 0x3 
[MCU2_0]     44.446065 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_CONFIG 
[MCU2_0]     44.446121 s: Application requested features = 0x158 
[MCU2_0]  
[MCU2_0]     44.446162 s: Disabling broadcast mode 
[MCU2_0]     44.446209 s: ub960InstanceId disableUB960: 0
[MCU2_0]     44.446247 s: UB960 config start 
[MCU2_0]     44.702094 s: End of UB960 config 
[MCU2_0]     44.702185 s: ub960InstanceId disableUB960: 1
[MCU2_0]     44.702222 s: UB960 config start 
[MCU2_0]     44.958098 s: End of UB960 config 
[MCU2_0]     44.958163 s: IM_SENSOR_CMD_CONFIG channel_mask = f
[MCU2_0]     44.958205 s: Configuring camera # 0 
[MCU2_0]     44.958252 s: Iss_sensor_isx016.c ...i am in ISX016_Config config script 
[MCU2_0]     44.958436 s: UB960 config start 
[MCU2_0]     44.962096 s: End of UB960 config 
[MCU2_0]     44.962151 s: ub953 config start : slaveAddr = 0x74 
[MCU2_0]     45.154161 s:  End of UB953 config 
[MCU2_0]     45.154277 s:  Configuring ISX016 imager 0x40.. Please wait till it finishes 
[MCU2_0]     45.473016 s:  ISX016 config done 
[MCU2_0]     45.473083 s:   iss_sensor_isx016.c ---> ISX016_Config finished 
[MCU2_0]     45.473125 s: Configuring camera # 1 
[MCU2_0]     45.473166 s: Iss_sensor_isx016.c ...i am in ISX016_Config config script 
[MCU2_0]     45.473357 s: UB960 config start 
[MCU2_0]     45.477097 s: End of UB960 config 
[MCU2_0]     45.477157 s: ub953 config start : slaveAddr = 0x76 
[MCU2_0]     45.669161 s:  End of UB953 config 
[MCU2_0]     45.669259 s:  Configuring ISX016 imager 0x42.. Please wait till it finishes 
[MCU2_0]     46.003015 s:  ISX016 config done 
[MCU2_0]     46.003087 s:   iss_sensor_isx016.c ---> ISX016_Config finished 
[MCU2_0]     46.003129 s: Configuring camera # 2 
[MCU2_0]     46.003169 s: Iss_sensor_isx016.c ...i am in ISX016_Config config script 
[MCU2_0]     46.003360 s: UB960 config start 
[MCU2_0]     46.007098 s: End of UB960 config 
[MCU2_0]     46.007158 s: ub953 config start : slaveAddr = 0x78 
[MCU2_0]     46.199169 s:  End of UB953 config 
[MCU2_0]     46.199267 s:  Configuring ISX016 imager 0x44.. Please wait till it finishes 
[MCU2_0]     46.518018 s:  ISX016 config done 
[MCU2_0]     46.518087 s:   iss_sensor_isx016.c ---> ISX016_Config finished 
[MCU2_0]     46.518127 s: Configuring camera # 3 
[MCU2_0]     46.518167 s: Iss_sensor_isx016.c ...i am in ISX016_Config config script 
[MCU2_0]     46.518359 s: UB960 config start 
[MCU2_0]     46.522100 s: End of UB960 config 
[MCU2_0]     46.522159 s: ub953 config start : slaveAddr = 0x7a 
[MCU2_0]     46.714185 s:  End of UB953 config 
[MCU2_0]     46.714283 s:  Configuring ISX016 imager 0x46.. Please wait till it finishes 
    47.033340 s: ISS: Initializing sensor [ISX016-UB913] ... Done !!!
Sensor init done!
entered configure_capture_params 
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
APP_BUFFER_Q_DEPTH : 4
APP_PIPELINE_DEPTH : 7
Capture init done!
app_init_color_conv() : ENTERING 
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
app_init_color_conv() : EXITING 
Color Conv init done!
[LDC-MODULE] configure_dcc_params() : ENTERING
[LDC-MODULE] configure_dcc_params() : Setting DCC config object to NULL! 
[LDC-MODULE] configure_dcc_params() : EXITING
[MCU2_0]     47.033019 s:  ISX016 config done 
[MCU2_0]     47.033089 s:   iss_sensor_isx016.c ---> ISX016_Config finished 
[MCU2_0]     47.033127 s: IM_SENSOR_CMD_CONFIG returning status = 0
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
LDC init done!
create_scaler_outputs vxGetStatus:0inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
create_scaler_outputs vxGetStatus:0inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Scaler init done!
Computing checksum at 0x0000FFFFAFE604C0, size = 12712900
TIDL Init Done! 
preProcObj->num_input_tensors:1
Pre Proc Update Done! 
Pre Proc Init Done! 
APP_INIT Number of Input Tensors in draw detections 3
PostProc Update Done! 
after vxCreateObjectArray
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
after vxReleaseImage
PostProc Init Done! 
Img Mosaic init done!
Display init done!
inside vxVerifyGraph above for loop
inside vxVerifyGraph after for loop
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
before ownReferenceUnlock
after ownReferenceUnlock
above ownReleaseMetaFormat for loop
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
end of vxVerifyGraph
after app_init  
App Init Done! 
before  app_create_graph 
 app_create_graph() : ENTERING 
Graph create done!
Capture graph done!
app_create_graph_color_conv() : ENTERING 
Color convert node create started
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Color convert node create done 
app_create_graph_color_conv() : EXITING 
Color Conversion graph done!
[LDC-MODULE] app_create_graph_ldc() : ENTERING 
[LDC-MODULE] app_create_graph_ldc() : DCC config object is NULL 
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
[LDC-MODULE] Created LDC node without DCC config and NULL mesh_config! 
[LDC-MODULE] app_create_graph_ldc() : EXITING 
LDC graph done!
inside if above replicates
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
exiting app_create_graph_scaler
Scaler graph done!
vxQueryNode num_params value:3
before vxReplicateNode
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
after vxReplicateNode
before vxReleaseImage
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
after vxReleaseImage
before vxReleaseTensor
after vxReleaseTensor
Pre proc graph done!
app_create_graph_tidl num_input_tensors:1 and num_output_tensors:3
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
after vxReleaseTensor input_tensor
after vxReleaseTensor output_tensor
TIDL graph done!
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
vxQueryObjectArray items value:4
after vxReplicateNode num_input_tensors in postproc:3
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
PostProc graph done!
Img Mosaic graph done!
Display graph done!
 app_create_graph : Exiting 
after  app_create_graph 
App Create Graph Done! 
before  app_verify_graph 
before vxVerifyGraph(obj->graph)
;inside vxVerifyGraph above for loop
inside vxVerifyGraph after for loop
1
2
3
4
5
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
6
7
8
9
10
11
12
13
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
14
15
16
17
    47.766848 s:  VX_ZONE_ERROR:[ownContextSendCmd:799] Command ack message returned failure cmd_status: -7
    47.766859 s:  VX_ZONE_ERROR:[ownContextSendCmd:835] tivxEventWait() failed.
    47.766866 s:  VX_ZONE_ERROR:[ownNodeKernelInit:527] Target kernel, TIVX_CMD_NODE_CREATE failed for node PreProcNode
    47.766871 s:  VX_ZONE_ERROR:[ownNodeKernelInit:528] Please be sure the target callbacks have been registered for this core
[C6x_1 ]     47.766736 s:  VX_ZONE_ERROR:[ownTargetKernelInstanceAlloc:116] kernel com.ti.img_proc.img.preprocess has not been registered on this CPU
    48.096107 s:  VX_ZONE_ERROR:[ownNodeKernelInit:529] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
[C6x_1 ]     47.766761 s:  VX_ZONE_ERROR:[ownTargetKernelInstanceAlloc:117] Please register this kernel on the appropriate target core
[C6x_1 ]     47.766781 s:  VX_ZONE_ERROR:[ownTargetNodeDescNodeCreate:761] target_kernel_instance is NULL
    48.096218 s:  VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 4, kernel com.ti.img_proc.img.preprocess ... failed !!!
    48.096233 s:  VX_ZONE_ERROR:[vxVerifyGraph:2058] Node kernel init failed
18
19
20
21
22
23
    48.096253 s:  VX_ZONE_ERROR:[vxVerifyGraph:2112] Graph verify failed
24
before ownReferenceUnlock
after ownReferenceUnlock
above ownReleaseMetaFormat for loop
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
[MCU2_0]     48.096448 s: ==========================================================
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
[MCU2_0]     48.096546 s:  Capture Status: Instance|0
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
[MCU2_0]     48.096581 s: ==========================================================
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
[MCU2_0]     48.096625 s:  overflowCount: 0
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
[MCU2_0]     48.096662 s:  spuriousUdmaIntrCount: 0
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
[MCU2_0]     48.096697 s:  frontFIFOOvflCount: 0
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
[MCU2_0]     48.096729 s:  crcCount: 0
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
[MCU2_0]     48.096758 s:  eccCount: 0
before ownReleaseMetaFormat
after ownReleaseMetaFormat
before ownReleaseMetaFormat
[MCU2_0]     48.096789 s:  correctedEccCount: 0
after ownReleaseMetaFormat
before ownReleaseMetaFormat
after ownReleaseMetaFormat
[MCU2_0]     48.096822 s:  dataIdErrorCount: 0
end of vxVerifyGraph
after vxVerifyGraph(obj->graph)
;Grapy verify FAILURE!
[MCU2_0]     48.096856 s:  invalidAccessCount: 0
[MCU2_0]     48.096890 s:  invalidSpCount: 0
[MCU2_0]     48.096928 s:  strmFIFOOvflCount[0]: 0
[MCU2_0]     48.096967 s:  strmFIFOOvflCount[1]: 0
[MCU2_0]     48.097080 s:  Channel Num | Frame Queue Count | Frame De-queue Count | Frame Drop Count | Error Frame Count |
[MCU2_0]     48.097164 s:            0 |                 0 |                    0 |                0 |                 0 |
[MCU2_0]     48.097241 s:            1 |                 0 |                    0 |                0 |                 0 |
[MCU2_0]     48.097315 s:            2 |                 0 |                    0 |                0 |                 0 |
[MCU2_0]     48.097390 s:            3 |                 0 |                    0 |                0 |                 0 |
after app_verify_graph  
App Verify Graph Done! 
App Run Graph Done! 
before  app_delete_graph 
Capture delete done!
Color Conv delete done!
LDC delete done!
Scaler delete done!
Pre Proc delete done!
TIDL delete done!
Post Proc delete done!
Img Mosaic delete done!
Display delete done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Graph delete done!
after  app_delete_graph 
App Delete Graph Done! 
before app_deinit  
start of de-init
    48.531929 s: ISS: De-initializing sensor [ISX016-UB913] ... !!!
    48.532311 s: ISS: De-initializing sensor [ISX016-UB913] ... Done !!!
Sensor deinit done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Capture deinit done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Color Conv deinit done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
LDC deinit done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Scaler deinit done!
Pre proc deinit done!
TIDL deinit done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
RCI PostProc deinit done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
inside vxReleaseImage
inside ownIsValidSpecificReference                                                                                    
above ownReleaseReferenceInt                                                                                          
inside vxReleaseImage                                                                                                 
inside ownIsValidSpecificReference                                                                                    
above ownReleaseReferenceInt                                                                                          
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Img Mosaic deinit done!
Display deinit done!
inside vxReleaseImage
inside ownIsValidSpecificReference
above ownReleaseReferenceInt
Graphics deinit Done! 
Kernels unload done!
    49.255395 s:  VX_ZONE_WARNING:[vxReleaseContext:1055] Found a reference 0xffffbbd201c8 of type 00000804 at external count 1, internal count 1, releasing it
    49.255404 s:  VX_ZONE_WARNING:[vxReleaseContext:1057] Releasing reference (name=com.ti.color_conv_kernel.color_conv_example) now as a part of garbage collection
    49.255410 s:  VX_ZONE_WARNING:[vxReleaseContext:1066] A kernel with name com.ti.color_conv_kernel.color_conv_example has not been removed, possibly due to a kernel module not being unloaded.
    49.255416 s:  VX_ZONE_WARNING:[vxReleaseContext:1067] Removing as a part of garbage collection
    49.255426 s:  VX_ZONE_WARNING:[vxReleaseContext:1055] Found a reference 0xffffbbe16690 of type 00000815 at external count 1, internal count 0, releasing it
    49.255433 s:  VX_ZONE_WARNING:[vxReleaseContext:1057] Releasing reference (name=tidl_node_output_tensors_1) now as a part of garbage collection
    49.255442 s:  VX_ZONE_WARNING:[vxReleaseContext:1055] Found a reference 0xffffbbe168b0 of type 00000815 at external count 1, internal count 0, releasing it
    49.255449 s:  VX_ZONE_WARNING:[vxReleaseContext:1057] Releasing reference (name=tidl_node_output_tensors_2) now as a part of garbage collection
Release context done!
after app_deinit  
App De-init Done! 
Main end    49.255490 s:  VX_ZONE_INIT:[tivxHostDeInitLocal:107] De-Initialization Done for HOST !!!
    49.259854 s:  VX_ZONE_INIT:[tivxDeInitLocal:211] De-Initialization Done !!!
APP: Deinit ... !!!
REMOTE_SERVICE: Deinit ... !!!
REMOTE_SERVICE: Deinit ... Done !!!
IPC: Deinit ... !!!
IPC: DeInit ... Done !!!
MEM: Deinit ... !!!
DDR_SHARED_MEM: Alloc's: 78 alloc's of 62262960 bytes 
DDR_SHARED_MEM: Free's : 78 free's  of 62262960 bytes 
DDR_SHARED_MEM: Open's : 0 allocs  of 0 bytes 
DDR_SHARED_MEM: Total size: 536870912 bytes 
MEM: Deinit ... Done !!!
APP: Deinit ... Done !!!
root@j7-evm:/opt/vision_apps# 

The error is occurring at the below snippet in vxVerifyGraph function inside the app_verify_graph funcation call.

printf("17\n");
if(status == (vx_status)VX_SUCCESS)
{
/* Call target kernel init for each node
* This results in message coomunication with target kernels
* Memory gets allocated which MUST be free'ed via target kernel
* deinit.
* kernel deinit called during node release
*/
status = ownGraphNodeKernelInit(graph);
if(status != (vx_status)VX_SUCCESS)
{
VX_PRINT(VX_ZONE_ERROR,"Node kernel init failed\n");
}
}
printf("18\n");

Kindly let me know how to resolve the error.

Regards,

Chaitanya Prakash Uppala