This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6A816x: Errata with Advisory 1.1.18 CPGMAC 1-Gbps Mode Does Not Work When EMAC_TXCLK is Not Running.



We have used TMS320C6A816x EMCA0 as GMII and EMAC1 as MII port. Among these EMAC0 GMII PHY doesn’t provide TXCLK.

The errata says that 1Gbps mode will not work in case of TXCLK is not available. 

Question: Is this applicable only in case of Ethernet boot? Or TXCLK has to be driven all the time to make 1Gbps work.

(We are booting system from NAND Flash)

Thx,

Mihir Shah