This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM64: Flash SOC Initialization Binary failed in AM64-SK GP device

Part Number: SK-AM64
Other Parts Discussed in Thread: UNIFLASH

Hi,

     I'm new to MCU+SDK trying to learn as part of it to run and load few examples in AM64X-SK while flashing SOC initialization Binary i'm facing issues since im using the GP Please help me to resolve this.

C:\ti\mcu_plus_sdk_am64x_09_01_00_41\tools\boot\socid_parser>python uart_boot_socid.py -d am64x --string=01000000011a0000616d36347800000000000000475020200000010000000100
-----------------------
SoC ID Header Info:
-----------------------
NumBlocks            : 1
-----------------------
SoC ID Public ROM Info:
-----------------------
SubBlockId           : 1
SubBlockSize         : 26
DeviceName           : am64x
DeviceType           : GP
DMSC ROM Version     : [0, 1, 0, 0]
R5 ROM Version       : [0, 1, 0, 0]

C:\ti\mcu_plus_sdk_am64x_09_01_00_41\tools\boot>python uart_uniflash.py -p COM8 --cfg=sbl_prebuilt/am64x-sk/default_sbl_null.cfg

 

Parsing config file ...
Parsing config file ... SUCCESS. Found 2 command(s) !!!

 

Executing command 1 of 2 ...
Found flash writer ... sending sbl_prebuilt/am64x-sk/sbl_uart_uniflash.release.hs_fs.tiimage
Sent flashwriter sbl_prebuilt/am64x-sk/sbl_uart_uniflash.release.hs_fs.tiimage of size 329349 bytes in 31.97s.

 

Executing command 2 of 2 ...
Command arguments : --file=sbl_prebuilt/am64x-sk/sbl_null.release.hs_fs.tiimage --operation=flash --flash-offset=0x0
Sending sbl_prebuilt/am64x-sk/sbl_null.release.hs_fs.tiimage:   0%|                      | 0/296021 [00:00<?, ?bytes/s]send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'1'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'1'
send error: error_count reached 10, aborting.
Sending sbl_prebuilt/am64x-sk/sbl_null.release.hs_fs.tiimage:   0%|         | 2/296021 [01:30<7424:05:16, 90.29s/bytes]
[ERROR] XMODEM send failed, no response OR incorrect response from EVM OR cancelled by user,
Power cycle EVM and run this script again !!!

Thanks,

Prasanth S