Could the four channel CAN interfaces on the TDA4 EVM be all controlled by program of MCU sides?
Now, I have to complete the task, which is communication with VN1640(CANoe)by these four channels on the MCU side. So I need to figure out the details about four channel CAN distribution among the CORE<mpu1_0, mcu1_0, mcu1_1, mcu2_0, mcu2_1, mcu3_0, mcu3_1> to control.
For example, is it possible that all CAN channels could be control by single core MCU1_0?