Part Number: AM5726
In SPRUHZ6L it states:
NOTE: Only DSP_CLK3 clock is supported on this SoC. Upon boot time, sysboot15 set at '1' selects
a DSP_CLK3 divided clock version for the DSP subsystem logic and bus interfaces. For
SR1.1, sysboot15 must be tied to vdd to select DSP_CLK3, but for SR2.0 it is configurable.
For more information, see Section 18.4.6.1.1.1, Permanent PU/PD disabling (SR 2.0 only) in
Chapter 18, Control Module.
AND also:
15 DSP_CLOCK_DIVIDER SR1.x Only:
Divide factor for DSP clock
0x0: DSP_CLK2 is selected. Not supported on this SoC.
0x1: DSP_CLK3 is selected
SR2.0 Only:
Permanently disables the internal PU/PD resistors on pads
gpmc_a[27:24, 22:19].
0x0: Internal pull-down resistors are enabled
0x1: Internal pull-down resistors are permanently disabled
Does this mean that SYSBOOT15 has no effect on DSP_CLK for SR2.0?
So, for SR2.0, the DSP subsystem clock is NOT divided by 2 or 3 relative to the DSP DPLL output?