Other Parts Discussed in Thread: AM623,
Hello,
We have to prototype using AM62x.
Proto A using AM623 GP
Proto B using AM625 HS-FS
When using the same Linux SDK86 boot file the SD Card boot on Proto A but doesn't boot on proto B.
Here is the message :
U-Boot SPL 2021.01-g2ee8efd654 (Dec 04 2023 - 15:21:37 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from MMC2
mmc fail to send stop cmd
spl_load_image_fat: error reading image tispl.bin, err - -2
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
So switching to tftp boot on ethernet with the same file then proto B boot and go to u-boot prompt.
Here is the mmc info of the SD Card :
=> mmc info (Verbatim PROTO B u-boot sdk86)
Device: mmc@fa00000
Manufacturer ID: 27
OEM: 5048
Name: SD16G
Bus Speed: 200000000
Mode: UHS SDR104 (208MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.4 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
Could you confirm that the AM623 GP and AM625 HS-FS is managing the SD Card the same way.
Could you help us to fix this critical issue?
Regards,
Alexis.