Part Number: TMS320DM648
Hi, where can I get the BSDL file for TMS320DM648?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320DM648
Hi, where can I get the BSDL file for TMS320DM648?
Hello Vedant Khasakia
Thank you for the query.
Please refer below link and let me know if this helps.
https://www.ti.com/product/TMS320DM648#design-tools-simulation
Regards,
Sreenivasa
Hi,
Thank you for the response.
I see that there are two bsdl files available. Which one should I use?
Hello Vedant Khasakia
I would suggest using Rev A as i check internally on the difference.
Regards,
Sreenivasa
Hello Vedant Khasakia
Please refer additional inputs:
I downloaded both models and looked and it appears that the version 1.1 (sprm 361) is the more updated version for Silicon rev 1.1.
So if the customer is using silicon rev 1.1 I would point them to sprm361.
However if the customer is using the older silicon rev, the other one (sprm 256a) should be the one they need to use.
Regards,
Sreenivasa