This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168: DDR3 Configuration

Hi forum,

I have questions about the DDR3 device configuration in DM8168.
Target to build 2GByte total address space.

(1) To achieve this, is 8 x 2Gb devices the only config?
In this case, the connection can follow that of Netra EVM, Fig 8-14 in DS and Fig 7-9 in TRM.
Just the device is changed to Micron MT41J256M8HX.

(2) When study NETRA EVM, there are some resistor arrays in DDR data bus.
The bit mapping is different from a simple one. From the diagrams, I thought Byte[7]->DQ[7], Byte[6]->DQ[6], and so on.
Is there any special purpose to do so? Should I follow the same mapping as NETRA EVM?

(3) Any recommended material about routing and advice?

Thanks for your quick help and support.

Best regards,
Alex