This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J784S4: I need the GPU 23.1 driver

Part Number: PROCESSOR-SDK-J784S4
Other Parts Discussed in Thread: TDA4VH

Tool/software:

Need to port GPU support on TDA4VH, could you please provide the IMG DDK patch including build configurations for TI TDA4VH(J784S4) (version: 23.1.6404501)

Thanks.

  • Hello,

    I will need some more details on what you are trying to do:

    1) Which SDK version are you currently using?

    2) Which GPU driver version do you want to use? Are you trying to get the latest version? Is this for bug fixes or feature updates?

    Regards,

    Erick

  • Hi Erick,

    We will use PROCESSOR-SDK-LINUX-J784S4 09.02.
    This SDK includes the latest GPU kernel space driver - 23.3.6512818. It includes some feature updates and bug fixes.
    However, we don't have the user space source code of the latest version. Therefore, need TI provide the full source code of IMG DDK including build configurations (version: 23.3.6512818)

    We do have both kernel and user space source code from IMG which version is 23.1.6404501 but there's no configurations for TI TDA4VH, if TI can provide the configurations for that version and confirm working, that can also be a solution, thanks.

    Regards,

    Shawn

  • Shawn,

    I understand the situation now. Because of the proprietary nature of the UM source code, I cannot provide many details on the public forum. Can you please contact me through the email I private messaged you?

    Thanks,

    Erick