Tool/software:
Dear TI,
I am trying to run the T Eye firmware for DDR eye measurement. I am trying it out on an EVM, later I want to use my own custom board.
The readme says at point 4: "Connect to the SMS0_TIFS_0 core". I did that using CCS (the core is called SMS_CM4_0_TIFS_0 on this SoC), but I get the following error:
SMS_CM4_0_TIFS_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
What can I do against this error? I tried it both with booted Linux and unbooted, but the error is the same in both cases.
Many thanks
Leon Rigoni