Hi,
I've got a very power sensitive design started, and was therefore hoping to use the new Micron LPDDR2 memory, (eg MT42L128M16D1) on my DM8168 design (planning to use DM8165 in production). What I am curious about is whether the LPDDR2 would be supported, given that the datasheet implies 1.8V for DDR2 and 1.5V for DDR3, but LPDDR2 is 1.2V. I haven't checked through all the details yet, but I assume that it would then follow most of the other DDR2 specs, and it seems to meet the specs re address/cs/clk lines etc.
I was wondering if I just applied 1.2V to the DDR_VDD pins and 0.6V to the DDR Vref pins whether it would work, or am I being grossly optimistic?
Cheers,
Simon