When calling the Stream_control second time I get following error dump? Any clue as to how I can debug this exception? I am using BIOS 6.32.02.39 and PSP 2.20.01.01. The first call goes through fine.
A0=0x0 A1=0x1
A2=0xffff011e A3=0x8b10899c
A4=0x0 A5=0x8b0b7900
A6=0x80680009 A7=0x887cc100
A8=0x8b101c84 A9=0x8f000000
A10=0xff9f A11=0x8b104c88
A12=0xffffffff A13=0x8b108a6c
A14=0x8b108a78 A15=0x8b151708
A16=0x1000000 A17=0x0
A18=0x8b104354 A19=0x20
A20=0x0 A21=0x0
A22=0xf5a9b34b A23=0xccdbba6c
A24=0xf959ef64 A25=0xb77f8ff2
A26=0xf75dd3fb A27=0xb7ea6e73
A28=0x18023802 A29=0x20
A30=0x20 A31=0x0
B0=0x1 B1=0x0
B2=0x0 B3=0x8b0b7ae8
B4=0x0 B5=0x0
B6=0x8b1089b4 B7=0x8b1389f0
B8=0x8b108a78 B9=0x0
B10=0x1 B11=0x1
B12=0x8c8007b0 B13=0x1
B14=0x8b1524c0 B15=0x8b108908
B16=0x4 B17=0x8b104610
B18=0xa B19=0x78
B20=0x69 B21=0xf8177fa2
B22=0xf B23=0x0
B24=0xaafeb6f9 B25=0x3912bde6
B26=0xfffffffe B27=0x994a35b5
B28=0x1e9a173f B29=0x1e9a173f
B30=0x8e000780 B31=0x14
NTSR=0x1020f
ITSR=0x20f
IRP=0x8b089964
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x0
EFR=0x2 NRP=0x0
Internal exception: IERR=0x1
Instruction fetch exception
[t=0x00000029:b6008ce3] [tid=0x8b107ad8] ti.sysbios.family.c64p.Exception: ERROR: line 248: E_exceptionMin: pc = 0x8b089964, sp = 0x8b108908.
ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x8b089964, sp = 0x8b108908.
xdc.runtime.Error.raise: terminating execution