I've been able to run my program on both displays independently with the same timings, but not simultaniously.
Here is a snippit script that I'm running:
modprobe vpss sbufaddr=0xBFB00000 mode=hdmi:1080p-60 debug=1 i2c_mode=1
modprobe ti81xxfb vram=0:24M,1:16M,0:6M
echo 5 > /sys/devices/platform/vpss/system/tiedvencs
echo 2:hdmi,dvo2 > /sys/devices/platform/vpss/graphics0/nodes
echo 0 > /sys/devices/platform/vpss/display0/enabled
echo 0 > /sys/devices/platform/vpss/display1/enabled
echo 75010,1366/50/77/30,768/7/19/5,1 > /sys/devices/platform/vpss/display0/timings
echo 75010,1366/50/77/30,768/7/19/5,1 > /sys/devices/platform/vpss/display1/timings
echo 1 > /sys/devices/platform/vpss/display0/enabled
echo 1 > /sys/devices/platform/vpss/display1/enabled
fbset -xres 1366 -yres 768 -vxres 1366 -vyres 768
fbset -depth 32 -rgba 8/16,8/8,8/0,0/0
modprobe ti81xxhdmi
And this is the output I am getting:
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
Setting Timing
ti81xxfb ti81xxfb: failed to star.
open /dev/fb0: No such process
ti81xxfb ti81xxfb: failed to star.
open /dev/fb0: No such process
HDMI W1 rev 2.0
ti81xxfb ti81xxfb: failed to star.
./vpss.sh: line 65: can't create /dev/fb0: No such process
Is there somthing that I am missing?
Thanks,
-Jared Falter