Part Number: AM3358
Tool/software:
Hi Team,
Wanted to check if the given devices are UL Certified:
AM3358BZCZ100 & TMS320F28379DPTPT
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3358
Tool/software:
Hi Team,
Wanted to check if the given devices are UL Certified:
AM3358BZCZ100 & TMS320F28379DPTPT
Regards
Hello,
If this in reference to safety UL certification: We do not provide certification for TI provided hardware or software to the IEC 60730 Class B and UL 1998 Class 1 and this is typically done at the system level. Requirements in these specs are derived from the IEC 61508 and the TI devices depending on the process are certified for IEC 61508 SIL-2/ISO-26262 ASIL-B (systematic capability of ASIL-D/SIL-3).
Best,
Mahir Kaheri