Other Parts Discussed in Thread: OMAPL138, SYSBIOS
URGENT
Hello friends,
Recently I am getting a loading error in CCSv4.2.4 . I am targeting C6748/OMAPL138 SoM and attached ..\gel\OMAPL138_DSP to DSP/OMAPL138 and ..\gel\TI_Update_OMAPL138_ARM.gel to ARM/OMAPL138. These are recent files downloaded from LogicPD. I am showing the screen shot below,
This
is CCSV4.2.4, SysBIOS(default). I refer to document “SPRS586B–JUNE 2009–REVISED
AUGUST 2010” the table 3-4 , this address is corresponding to
DDR2 data memory on DSP side. How to use this information and modify the gel file. Is it required at all?
When I change the GEL file to C6748.gel from OMAPL138_DSP .gel it is loading the file but audio is not getting acquired.I can perceive a click sound but not the music/audio. I cross verified the hardware and all the software set up by running the logicPd audio test program and find that they are working for both C6748.gel and OMAPL138_DEP.gel.
I am in state of confusion and I sincerely request somebody from forum to resolve this problem today.
Thank you
With best regards,
Prat