Part Number: AM625
Tool/software:
Hello Ti experts,
Recently I've built an Android for AM625 using SDK V10.00 with Kernel V6.1 as well as V6.6
But, in both the cases my custom AM625 SOM is not booting fully with new Android build.
It gets stuck on android boot-screen and in logs there is a line which it prints continuously. I've attached the booting logs for your reference.
Kindly help as soon as possible.
These are the booting logs.
U-Boot SPL 2023.04 (Aug 06 2024 - 14:18:45 +0200) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13392 bytes Trying to boot from MMC1 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):09.02.00.009 NOTICE: BL31: Built : 14:18:41, Aug 6 2024 U-Boot SPL 2023.04 (Aug 06 2024 - 14:19:09 +0200) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 1904 bytes Trying to boot from MMC1 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2023.04 (Aug 06 2024 - 14:19:09 +0200) SoC: AM62X SR1.0 GP Model: Texas Instruments AM625 SK EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -1 DRAM: 2 GiB Core: 70 devices, 30 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from MMC... OK In: serial Out: serial Err: serial EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -1 Net: Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000port@1: phy_connect() failed No ethernet found. Hit any key to stop autoboot: 0 Verify GPT: success! Loading Android boot partition... switch to partitions #0, OK mmc0(part 0) is current device misc partition number:0x3 ANDROID: Invalid CRC-32 (expected 807077e9, found 00000000),re-initializing A/B metadata. ANDROID: Attempting slot a, tries remaining 7 ANDROID: Booting slot: a A/B cmdline addition: androidboot.slot_suffix=_a Running without AVB... MMC read: dev # 0, block # 29696, count 81920 ... 81920 blocks read: OK MMC read: dev # 0, block # 193536, count 65536 ... 65536 blocks read: OK Preparing FDT... Reading DTB for am62x_skevm... Working FDT set to 88000000 MMC read: dev # 0, block # 357376, count 16384 ... 16384 blocks read: OK Applying DTBOs... Running Android... ## Booting Android Image at 0x82000000 ... Kernel load addr 0x92000000 size 16888 KiB Kernel extra command line: console=ttyS2,115200 cma=512M 8250.nr_uarts=10 printk.devkmsg=on init=/init quiet firmware_class.path=/vendor/firmware mem_sleep_default=deep bootconfig RAM disk load addr 0xe9000000 size 14746 KiB ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Uncompressing Kernel Image Loading Ramdisk to 8f199000, end 8ffff7ec ... OK Loading Device Tree to 000000008f187000, end 000000008f198b1f ... OK Working FDT set to 8f187000 Starting kernel ... [ 0.560796][ T84] debugfs: Directory 'pd:186' with parent 'pm_genpd' already present! [ 0.562445][ T84] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present! [ 0.611146][ T85] ti-sci-clk 44043000.system-controller:clock-controller: recalc-rate failed for dev=81, clk=20, ret=-19 [ 0.779222][ T53] pinctrl-single f4000.pinctrl: pin PIN117 already requested by 2820000.serial; cannot claim for 1-0022 [ 0.790228][ T53] pinctrl-single f4000.pinctrl: pin-117 (1-0022) status -22 [ 0.790243][ T53] pinctrl-single f4000.pinctrl: could not request pin 117 (PIN117) from group main-gpio1-ioexp-intr-pins-default on device pinctrl-single [ 0.790252][ T53] pca953x 1-0022: Error applying setting, reverse things back [ 0.940275][ T1] init: Failed to copy /avb into /metadata/gsi/dsu/avb/: No such file or directory [ 1.940584][ T1] init: [libfs_avb] Invalid hash size: [ 1.946106][ T1] init: [libfs_avb] Failed to verify vbmeta digest [ 2.017552][ T1] logwrapper: Cannot log to file /dev/fscklogs/log [ 2.019767][ T125] logwrapper: executing /system/bin/e2fsck failed: No such file or directory [ 2.023972][ T1] logwrapper: [ 2.032590][ T125] logwrapper: [ 2.264632][ T1] init: Could not update logical partition [ 2.270779][ T1] init: Could not update logical partition [ 2.281326][ T1] init: Failed to open package /system/etc/selinux/apex/SEPolicy.zip: No such file or directory [ 2.550708][ T1] selinux: SELinux: Could not stat /dev/selinux: No such file or directory. [ 2.756203][ T1] selinux: SELinux: Could not get canonical path for /metadata/ota/rollback-indicator restorecon: No such file or directory. [ 2.769291][ T1] selinux: SELinux: Could not stat /metadata/gsi: No such file or directory. [ 3.111802][ T132] apexd: Failed to scan /system_ext/apex : Can't open /system_ext/apex for reading : No such file or directory [ 3.123787][ T132] apexd: Failed to scan /product/apex : Can't open /product/apex for reading : No such file or directory [ 3.135296][ T132] apexd: Failed to scan /vendor/apex : Can't open /vendor/apex for reading : No such file or directory [ 3.193901][ T134] ueventd: LoadWithAliases was unable to load platform:reg-dummy [ 3.204618][ T137] ueventd: LoadWithAliases was unable to load platform:ti-cpufreq [ 3.204691][ T134] ueventd: LoadWithAliases was unable to load of:Nregulator-2T(null)Cregulator-fixed [ 3.205658][ T135] ueventd: LoadWithAliases was unable to load of:Nregulator-7T(null)Cregulator-fixed [ 3.207690][ T135] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.214301][ T137] ueventd: LoadWithAliases was unable to load of:Nl2-cache0T(null)Ccache [ 3.224460][ T134] ueventd: LoadWithAliases was unable to load of:Nregulator-0T(null)Cregulator-fixed [ 3.234509][ T137] ueventd: LoadWithAliases was unable to load of:NramoopsT(null)Cramoops [ 3.242174][ T134] ueventd: LoadWithAliases was unable to load of:NbusT(null)Csimple-bus [ 3.250627][ T137] ueventd: LoadWithAliases was unable to load platform:Fixed MDIO bus [ 3.251535][ T136] ueventd: LoadWithAliases was unable to load of:NpsciT(null)Carm,psci-1.0 [ 3.252555][ T136] ueventd: LoadWithAliases was unable to load platform:snd-soc-dummy [ 3.254609][ T136] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.260164][ T134] ueventd: LoadWithAliases was unable to load of:NsramT(null)Cmmio-sram [ 3.268604][ T137] ueventd: LoadWithAliases was unable to load of:NledsT(null)Cgpio-leds [ 3.286526][ T134] ueventd: LoadWithAliases was unable to load mmc:block [ 3.337676][ T134] ueventd: LoadWithAliases was unable to load of:Ndss-oldi-io-ctrlT(null)Csyscon [ 3.337703][ T135] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.338632][ T136] ueventd: LoadWithAliases was unable to load of:NsysconT(null)CsysconCsimple-mfd [ 3.359783][ T135] ueventd: LoadWithAliases was unable to load of:NbusT(null)Csimple-pm-bus [ 3.373742][ T136] ueventd: LoadWithAliases was unable to load of:NpinctrlT(null)Cpinctrl-single [ 3.391318][ T134] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.392220][ T135] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.397008][ T136] ueventd: LoadWithAliases was unable to load of:Ndma-controllerT(null)Cti,am64-dmss-pktdma [ 3.402076][ T134] ueventd: LoadWithAliases was unable to load of:NusbT(null)Csnps,dwc3 [ 3.405038][ T134] ueventd: LoadWithAliases was unable to load of:Ndma-controllerT(null)Cti,am64-dmss-bcdma [ 3.407524][ T134] ueventd: LoadWithAliases was unable to load of:NpinctrlT(null)Cti,am6-padconf [ 3.410648][ T135] ueventd: LoadWithAliases was unable to load of:NbusT(null)Csimple-mfd [ 3.427112][ T136] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.458702][ T135] ueventd: LoadWithAliases was unable to load of:NbusT(null)Csimple-bus [ 3.458872][ T134] ueventd: LoadWithAliases was unable to load of:NpinctrlT(null)Cpinctrl-single [ 3.474174][ T135] ueventd: LoadWithAliases was unable to load of:NgpioT(null)Cti,am64-gpioCti,keystone-gpio [ 3.492566][ T135] ueventd: LoadWithAliases was unable to load of:NusbT(null)Csnps,dwc3 [ 3.502446][ T136] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode [ 3.502907][ T135] ueventd: LoadWithAliases was unable to load usb:v275Dp0BA6d0100dc00dsc00dp00ic03isc01ip02in00 [ 3.523260][ T134] Goodix-TS 2-005d: Error reading 1 bytes from 0x8140: -121 [ 3.524904][ T135] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.528731][ T135] ueventd: LoadWithAliases was unable to load of:NwatchdogT(null)Cti,j7-rti-wdt [ 3.551786][ T136] ueventd: LoadWithAliases was unable to load platform:xhci-hcd [ 3.561047][ T136] ueventd: LoadWithAliases was unable to load hid:b0003g0001v0000275Dp00000BA6 [ 3.563264][ T134] Goodix-TS 2-005d: Error reading 1 bytes from 0x8140: -121 [ 3.563493][ T135] ueventd: LoadWithAliases was unable to load of:NchipidT(null)Cti,am654-chipid [ 3.566232][ T135] ueventd: LoadWithAliases was unable to load of:Ntimer-cl0-cpu0T(null)Carm,armv8-timer [ 3.568638][ T135] ueventd: LoadWithAliases was unable to load of:Nregulator-3T(null)Cregulator-fixed [ 3.569445][ T135] ueventd: LoadWithAliases was unable to load platform:psci-cpuidle [ 3.570195][ T135] ueventd: LoadWithAliases was unable to load platform:serial8250 [ 3.571437][ T136] ueventd: LoadWithAliases was unable to load usb:v1D6Bp0002d0601dc09dsc00dp01ic09isc00ip00in00 [ 3.578239][ T55] k3-m4-rproc 5000000.m4fss: mbox_request_channel failed: -517 [ 3.591344][ T135] ueventd: LoadWithAliases was unable to load of:Nregulator-6T(null)Cregulator-fixed [ 3.596028][ T55] remoteproc remoteproc0: can't start rproc 5000000.m4fss: -16 [ 3.607180][ T135] ueventd: LoadWithAliases was unable to load cpu:type:aarch64:feature:,0000,0001,0002,0003,0004,0005,0006,0007,000B [ 3.607198][ T135] ueventd: [ 3.618044][ T134] Goodix-TS 2-005d: I2C communication failure: -121 [ 3.621554][ T134] ueventd: LoadWithAliases was unable to load of:NsysconT(null)CsysconCsimple-mfd [ 3.639067][ T136] ueventd: LoadWithAliases was unable to load of:Ni2cT(null)Cti,am64-i2cCti,omap4-i2c [ 3.697154][ T134] ueventd: LoadWithAliases was unable to load platform:alarmtimer [ 3.697370][ T136] ueventd: LoadWithAliases was unable to load of:NbusT(null)Csimple-bus [ 3.707291][ T134] ueventd: LoadWithAliases was unable to load of:NesmT(null)Cti,j721e-esm [ 3.715483][ T136] ueventd: LoadWithAliases was unable to load of:NsysconT(null)Csyscon [ 3.724316][ T134] ueventd: LoadWithAliases was unable to load of:Nopp-tableT(null)Coperating-points-v2-ti-cpu [ 3.743892][ T134] ueventd: LoadWithAliases was unable to load cpu:type:aarch64:feature:,0000,0001,0002,0003,0004,0005,0006,0007,000B [ 3.756205][ T136] k3_r5_rproc bus@f0000:bus@b00000:r5fss@78000000: SoC supports only single core R5 but num_cores is set to 0 [ 3.756345][ T134] ueventd: [ 3.760058][ T136] ueventd: LoadWithAliases was unable to load of:Nregulator-5T(null)Cregulator-fixed [ 3.797218][ T136] ueventd: LoadWithAliases was unable to load cpu:type:aarch64:feature:,0000,0001,0002,0003,0004,0005,0006,0007,000B [ 3.809485][ T136] ueventd: [ 3.848507][ T137] am65-cpsw-nuss 8000000.ethernet: Use random MAC address [ 3.869692][ T137] ueventd: LoadWithAliases was unable to load of:NtimerT(null)Cti,am654-timer [ 3.881188][ T137] ueventd: LoadWithAliases was unable to load of:NesmT(null)Cti,j721e-esm [ 3.897841][ T137] ueventd: LoadWithAliases was unable to load input:b0003v275Dp0BA6e0111-e0,1,2,4,k110,111,112,r0,1,8,B,am4,lsfw [ 3.924866][ T137] ueventd: LoadWithAliases was unable to load of:NwatchdogT(null)Cti,j7-rti-wdt [ 3.966943][ T137] ueventd: LoadWithAliases was unable to load of:NsysconT(null)Csyscon [ 3.979836][ T137] ueventd: LoadWithAliases was unable to load of:Ntarget-moduleT(null)Cti,sysc-omap2Cti,sysc [ 3.992692][ T137] ueventd: LoadWithAliases was unable to load of:Nregulator-1T(null)Cregulator-fixed [ 4.004707][ T137] ueventd: LoadWithAliases was unable to load of:Nregulator-8T(null)Cregulator-fixed [ 4.018970][ T137] ueventd: LoadWithAliases was unable to load of:NpmuT(null)Carm,cortex-a53-pmu [ 4.030422][ T137] ueventd: LoadWithAliases was unable to load cpu:type:aarch64:feature:,0000,0001,0002,0003,0004,0005,0006,0007,000B [ 4.042580][ T137] ueventd: [ 4.103613][ T131] ueventd: LoadWithAliases was unable to load of:Nm4fssT(null)Cti,am64-m4fss [ 4.162553][ T131] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 4.172103][ T131] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 4.184863][ T131] ueventd: LoadWithAliases was unable to load of:NcfgT(null)Cti,pruss-cfgCsyscon [ 4.234281][ T131] ueventd: LoadWithAliases was unable to load of:NpruT(null)Cti,am625-pru [ 4.250997][ T131] ueventd: LoadWithAliases was unable to load of:NprussT(null)Cti,am625-pruss [ 4.267521][ T131] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 4.361402][ T131] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null) [ 4.376499][ T131] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null)Cethernet-phy-id0007.c0f0Cethernet-phy-ieee802.3-c22 [ 4.394311][ T131] ueventd: LoadWithAliases was unable to load of:NmdioT(null)Cti,cpsw-mdioCti,davinci_mdio console:/ $ [ 4.517815][ T131] ueventd: LoadWithAliases was unable to load of:Ninterrupt-controllerT(null)Cti,pruss-intc [ 4.541546][ T131] ueventd: LoadWithAliases was unable to load of:NpruT(null)Cti,am625-pru [ 4.559067][ T131] ueventd: LoadWithAliases was unable to load of:NpruT(null)Cti,am625-pru [ 4.610879][ T158] cutils-trace: Error opening trace file: Permission denied (13) [ 8.055813][ T128] init: Unable to set property 'ro.boottime.init.fsck.data' from uid:0 gid:0 pid:171: Read-only property was already set [ 8.192435][ T128] init: Unable to set property 'ro.boottime.init.mount.data' from uid:0 gid:0 pid:171: Read-only property was already set [ 8.233702][ T1] init: Control message: Could not find 'aidl/android.system.keystore2.IKeystoreService/default' for ctl.interface_start from pid: 158 (/system/bin/servicemanager) [ 8.592707][ T171] vold: keystore2 Keystore earlyBootEnded returned service specific error: -100 [ 8.608959][ T128] init: Could not load single persistent property file, trying legacy directory: Unable to read persistent property file: open() failed: No such file or directory [ 8.737690][ T167] logd: Cannot read /data/misc/logd/event-log-tags [ 8.747843][ T167] logd: FrameworkListener: read() failed (Connection reset by peer) [ 11.131527][ T1] selinux: SELinux: Could not stat /data/dalvik-cache/arm: No such file or directory. [ 11.141562][ T1] selinux: SELinux: Could not stat /data/dalvik-cache/arm64: No such file or directory. [ 11.151735][ T1] selinux: SELinux: Could not stat /data/dalvik-cache/riscv64: No such file or directory. [ 11.162168][ T1] selinux: SELinux: Could not stat /data/dalvik-cache/x86: No such file or directory. [ 11.172154][ T1] selinux: SELinux: Could not stat /data/dalvik-cache/x86_64: No such file or directory. [ 14.812231][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) D/TA: TA_CreateEntryPoint:33 Checking master key secret D/TA: TA_CreateEntryPoint:38 Create master key secret [ 14.897168][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 15.845367][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 16.838074][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 17.839870][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 18.841690][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 19.843363][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 20.845553][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 21.847420][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 22.849264][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 23.851220][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 24.853315][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 25.854911][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 26.857883][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 27.859481][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 28.865354][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 29.865598][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 30.868938][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 31.873759][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 32.874834][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 33.877324][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 34.879713][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 35.881898][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 36.884055][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 37.886133][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 38.887878][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 39.890014][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 40.892598][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 41.894303][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 42.896670][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 43.916370][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 44.918333][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 45.455568][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 45.472634][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 45.919910][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 46.309334][ T131] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null)Cethernet-phy-id0007.c0f0Cethernet-phy-ieee802.3-c22 [ 46.340198][ T131] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null) [ 46.458767][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 46.921989][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 47.478475][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 47.931180][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 48.478638][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 48.932962][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 49.485888][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 49.939188][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 50.483800][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 50.933107][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 51.487552][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 51.944616][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 52.494071][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 52.939274][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 53.496530][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 53.962776][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 54.512762][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 54.951475][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 55.308932][ T158] servicemanager: VINTF HALs require names in the format type/instance (e.g. some.package.foo.IFoo/default) but got: suspend_control [ 55.523465][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 55.959902][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 56.568971][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 56.962399][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 57.530418][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 57.959310][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 58.536200][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 58.969020][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 59.405798][ T158] servicemanager: VINTF HALs require names in the format type/instance (e.g. some.package.foo.IFoo/default) but got: suspend_control [ 59.536463][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 59.979819][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 60.550318][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 60.980848][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 61.563345][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 61.980793][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 62.556059][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 62.974257][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 63.562228][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 63.977809][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 64.561692][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 64.979963][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 65.564382][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 65.980859][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 66.566847][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 66.982995][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 67.568404][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 67.985009][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 68.570072][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 68.986086][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 69.571542][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 69.987634][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 70.572954][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 70.988967][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 71.574396][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 71.990511][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 72.576233][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 72.992072][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 73.577538][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 73.993546][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 74.578899][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 74.994907][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 75.580896][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 75.996381][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 76.582355][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 76.997715][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 77.583798][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 77.999183][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 78.585286][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 79.000637][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 79.586724][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 80.002059][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 80.588353][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 81.003662][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 81.589877][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 82.005016][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 82.591707][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 83.006521][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 83.592959][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 84.008065][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 84.594317][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 85.009386][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 85.595895][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 86.010818][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 86.597275][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 87.012577][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager) [ 87.598886][ T1] init: Control message: Could not find 'android.hardware.usb.gadget@1.0::IUsbGadget/default' for ctl.interface_start from pid: 159 (/system/bin/hwservicemanager)
This is the boot-screen at which it stucks while booting

Best Regards,
Aditya T