Part Number: AM6421
Tool/software:
Hi
Customer will only use the SD card during boot (SDBOOT).
Therefore, UHS-I will not be required, so they only want to supply 3.3V to SD.
From the HW perspective, I have a question about terminal processing.
They want to connect VDDA_3P3_SDIO and cap_VDDSHV_MMC1 directly to GND because they only want to provide 3.3V to SD.
Is it appropriate for terminal processing?
From the SW point of view, I have a question about terminal processing.
The customer code does not plan to use UHS-I, but they want to use SDBOOT.
When using SDBOOT, is there any code for UHS-I executed in ROM code or SBL, and as a result, it becomes necessary to process the terminal for UHS-I?