Part Number: AM5728
Tool/software:
Hi,
I have made a QT GUI application, I have two systems one with a display and another without a display but when I run the same application on both the systems ,the one without display shows a high CPU usage with Weston -idle-time=0 occupying more than 60% of the CPU and total CPU usage going to more than 100 with the application. The one with the display shows the same as 0 CPU usage and my total usage in that system is around 10%.
I have a few doubts due to this , they are-
- How is it different for both the systems with same Weston configuration and weston.ini script.
- Since there is no feedback from the Panel and due to the DTS panel timing my processor thinks there is a display always connected right? this is confirmed by checking /dev/fb0 and with no drm errors in dmesg which is getting enumerated in both the devices.
- Is there a way to solve this issue and also why does this happen?
Please help us solve this issue at the earliest .
Regards
Roshan Rajagopal