Hello,
Does anyone know what is the simplest way to measure time on DSP 674 on Netra ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Alla,
There is no DSP 674. Which device do you mean to ask about?
Which board are you using, your own or an EVM?
What kind of time do you want to measure, GMT or DSP clock cycles or between two events or other?
Regards,
RandyP
Alla,
You can use the following in some cases:
#include <c6h.x>
unsigned int uCalTime, ulStartTime, uEndTime, uBenchTime;
main()
{
TSCL = 0;
ullStartTime = TSCL;
ullCalTime = TSCL;
ullCalTime -= ullStartTime;
ullStartTime = TSCL;
<code to be measured>
ullEndTime = TSCL;
ullBenchTime = ullEndTime - ullStartTime - ullCalTime;
}
But the TSC (described in CPU & Instruction Set Reference Guide) is 64-bits, while just the TSCL half will overflow every 4G cycles. If this is a problem, then you will need to use a full 64-bit access. The version above is useful in most cases.
Regards,
RandyP
If you need more help, please reply back. If this answers the question, please click Verify Answer , below.