Tool/software:
I am working on DMA transfer in BB Black using PRU. This code is provided in pru software support package for am335x (BB Black).
#include <stdint.h>
#include <pru_cfg.h>
volatile register uint32_t __R30;
volatile register uint32_t __R31;
/* 1D Transfer Parameters */
typedef struct {
uint32_t src;
uint32_t dst;
uint32_t chan;
} hostBuffer;
/* EDMA PARAM registers */
typedef struct {
uint32_t sam : 1;
uint32_t dam : 1;
uint32_t syncdim : 1;
uint32_t static_set : 1;
uint32_t : 4;
uint32_t fwid : 3;
uint32_t tccmode : 1;
uint32_t tcc : 6;
uint32_t : 2;
uint32_t tcinten : 1;
uint32_t itcinten : 1;
uint32_t tcchen : 1;
uint32_t itcchen : 1;
uint32_t privid : 4;
uint32_t : 3;
uint32_t priv : 1;
} edmaParamOpt;
/*typedef struct{
uint32_t src;
} edmaParamSrc;*/
typedef struct {
uint32_t acnt : 16;
uint32_t bcnt : 16;
} edmaParamABcnt;
/*typedef struct{
uint32_t dst;
} edmaParamDst;*/
typedef struct {
uint32_t srcbidx : 16;
uint32_t dstbidx : 16;
} edmaParamBidx;
typedef struct {
uint32_t link : 16;
uint32_t bcntrld : 16;
} edmaParamLnkRld;
typedef struct {
uint32_t srccidx : 16;
uint32_t dstcidx : 16;
} edmaParamCidx;
typedef struct {
uint32_t ccnt : 16;
uint32_t : 16;
} edmaParamCcnt;
typedef struct {
edmaParamOpt opt;
/*edmaParamSrc*/ uint32_t src;
edmaParamABcnt abcnt;
/*edmaParamDst*/ uint32_t dst;
edmaParamBidx bidx;
edmaParamLnkRld lnkrld;
edmaParamCidx cidx;
edmaParamCcnt ccnt;
} edmaParam;
/* This is a compiler hack so that the PRU knows where the parameters are stored
* This is effectively a pointer to DRAM
*/
#pragma LOCATION(buf, 0)
hostBuffer buf;
/* Addresses for Constant Table pointer registers
* CTBIR_0 -> C24 (PRU0 DRAM)
* CTBIR_1 -> C25 (PRU1 DRAM)
*/
#define CTBIR_0 (*(volatile uint32_t *)(0x22020))
#define CTBIR_1 (*(volatile uint32_t *)(0x22024))
/* EDMA Channel Registers */
#define CM_PER_BASE ((volatile uint32_t *)(0x44E00000))
#define TPTC0_CLKCTRL (0x24 / 4)
#define TPCC_CLKCTRL (0xBC / 4)
#define ON (0x2)
/* EDMA Channel Registers */
#define EDMA0_CC_BASE ((volatile uint32_t *)(0x49000000))
#define DMAQNUM0 (0x0240 / 4)
#define DMAQNUM1 (0x0244 / 4)
#define DCHMAP_10 (0x0128 / 4)
#define QUEPRI (0x0284 / 4)
#define EMR (0x0300 / 4)
#define EMCR (0x0308 / 4)
#define EMCRH (0x030C / 4)
#define QEMCR (0x0314 / 4)
#define CCERRCLR (0x031C / 4)
#define DRAE0 (0x0340 / 4)
#define DRAE1 (0x0348 / 4)
#define DRAE2 (0x0350 / 4)
#define DRAE3 (0x0358 / 4)
#define QWMTHRA (0x0620 / 4)
#define GLOBAL_ESR (0x1010 / 4)
#define GLOBAL_ESRH (0x1014 / 4)
#define GLOBAL_EECR (0x1028 / 4)
#define GLOBAL_EECRH (0x102C / 4)
#define GLOBAL_SECR (0x1040 / 4)
#define GLOBAL_SECRH (0x1044 / 4)
#define GLOBAL_IESR (0x1060 / 4)
#define GLOBAL_IESRH (0x1064 / 4)
#define GLOBAL_ICR (0x1070 / 4)
#define GLOBAL_ICRH (0x1074 / 4)
/* EDMA Shadow Region 1 */
#define ESR (0x2210 / 4)
#define ESRH (0x2214 / 4)
#define EESR (0x1030 / 4)
#define EECR (0x2228 / 4)
#define EECRH (0x222C / 4)
#define SECR (0x2240 / 4)
#define SECRH (0x2244 / 4)
#define IPR (0x2268 / 4)
#define IPRH (0x226C / 4)
#define ICR (0x2270 / 4)
#define ICRH (0x2274 / 4)
#define IESR (0x2260 / 4)
#define IESRH (0x2264 / 4)
#define IEVAL (0x2278 / 4)
#define IECR (0x2258 / 4)
#define IECRH (0x225C / 4)
/* EDMA PARAM registers */
#define PARAM_OFFSET (0x4000 / 4)
#define OPT 0x00
#define SRC 0x04
#define ACNT 0x100
#define BCNT 0x1
#define DST 0x0C
#define SRC_DST_BIDX 0x10
#define LINK_BCNTRLD 0x14
#define SRC_DST_CIDX 0x18
#define CCNT 0x1
#define COPY_LENGTH 32
void main(void)
{
hostBuffer hostData;
uint32_t channelMask;
uint16_t paramOffset;
edmaParam params;
volatile uint32_t *ptr;
volatile uint32_t *ptr_cm;
volatile edmaParam *pParams;
ptr = EDMA0_CC_BASE;
ptr_cm = CM_PER_BASE;
/* Clear SYSCFG[STANDBY_INIT] to enable OCP master port */
CT_CFG.SYSCFG_bit.STANDBY_INIT = 0;
ptr_cm[TPTC0_CLKCTRL] = ON;
ptr_cm[TPCC_CLKCTRL] = ON;
/* Load channel parameters from DRAM - loaded by host */
hostData.src = /*buf.src*/ 0x4A310000; //PRU Shared memory
hostData.dst = /*buf.dst*/ 0x4A310100; //PRU Shared memory
hostData.chan = /*buf.chan*/ 10;
channelMask = (1 << hostData.chan);
/* Map Channel 10 to PaRAM 10 */
ptr[DCHMAP_10] = (hostData.chan << 5);
/* Setup EDMA region access for Shadow Region 1 */
ptr[DRAE1] |= channelMask;
/* Clear channel event from EDMA event registers */
ptr[SECR] |= channelMask;
ptr[ICR] |= channelMask;
/* Enable channel interrupt */
ptr[IESR] |= channelMask;
/* Enable channel */
ptr[EESR] |= channelMask;
/* Clear event missed register */
ptr[EMCR] |= channelMask;
/* Setup channel to submit to EDMA TC0 */
ptr[DMAQNUM1] &= 0xFFFFF0FF;
/* Setup and store PaRAM set for transfer */
paramOffset = PARAM_OFFSET;
/* channel * 0x20, word address */
paramOffset += ((hostData.chan << 5) / 4);
params.lnkrld.link = 0xFFFF;
params.lnkrld.bcntrld = 0x0000;
params.opt.tcc = hostData.chan;
params.opt.tcinten = 1;
params.opt.itcchen = 1;
params.ccnt.ccnt = CCNT;
params.abcnt.acnt = ACNT;
params.abcnt.bcnt = BCNT;
params.bidx.srcbidx = 0x1;
params.bidx.dstbidx = 0x1;
params.src = hostData.src;
params.dst = hostData.dst;
pParams = (volatile edmaParam *)(ptr + paramOffset);
*pParams = params;
/* Trigger transfer */
ptr[ESR] = (channelMask);
/* Wait for transfer completion */
while (!(ptr[IPR] & channelMask)) {
}
/* Halt PRU core */
__halt();
}
What is the use of this code?
I am putting data using “sudo devmem2 0x4A310000 w 0x2”. But after running the above code (provided in pru software support package) and then checking 0x4A310100, it is blank. The value “0x2” is not present there. The outputs are provided below.
debian@BeagleBone:~$sudo devmem2 0x4A310000 (source)
/dev/mem opened.
Memory mapped at address 0xb6f33000.
Value at address 0x4A310000 (0xb6f33000): 0x2
debian@BeagleBone:~$ sudo devmem2 0x4A310100 (destination)
/dev/mem opened.
Memory mapped at address 0xb6f76000.
Value at address 0x4A310100 (0xb6f76100): 0x0
On 23/02/2025 it worked smoothly. But on 24/02/2025 it is not working.
what can be the reason? How to resolve this?