Tool/software:
From the build sheet, no support for USB Host and device boot. It is needed. Especially for customers who worked on AM62x using DFU for eMMC flash on production line.
From errata, there is some problem on DFU boot, but not say it can't be supported definitely.
#1. What is the conclusion if support DFU or not on this device?
#2. If yes, can do DFU boot on AM62L EVM in HW design? I tried to connect J19 to PC, can't detect USB device with below boot mode setting:
#3. Is there a short plan to support DFU in SDK?