Other Parts Discussed in Thread: TMS320C6747
I want to boot program from nandflash when I use the tms320c6747 chip,however I don't success.
I am used the AISGen for D800K003 tool to produce 'xxx.bin' file.the tool config as follow picture.
then I write into nandflash block 1(using the c6747 bootloader refer to). The program cannot boot.
the pinmux config and hardware is doesnot wrong.
And anything I doesnot do ? I don't know what to the nandflash block 0 ,do I have to write bootloader load into the block 0,then start the program by its.
I don't know to write the bootloader if this,can you give me the code or tell me how to write?
thank you.