Part Number: AM6422
Tool/software:
Hi.
MMCSD1:
Is there an option to select between different driver strength for:
a) 3.3V signaling
b) 1V8 (UHS-I) signaling
The "MMCSD1_CAPABILITIES" Register indicating that Driver Type A,C and D are not supported. However, this register is gets information from "MMCSD1_SS_CTL_CFG_3_REG" Register, where the corresponding bit fields are R/W type. So I can configure that. Does the device supporting driver types A,C and D?
Any other option to adjust driver strength?
regards,
Christian