AM67A: How to make U-boot boot the kernel from mmcblk0p2?

Part Number: AM67A

Tool/software:

Now I have divided the emmc into two partitions. mmcblk0p1 has been allocated 10M for storing private data, and the remaining space has been assigned to mmcblk0p2. Then I extracted the tisdk-edgeai-image-j722s-evm.rootfs-20250918010209.tar.xz file to mmcblk0p2. Now I am unable to boot from the emmc. Where should I make the correction?

U-Boot SPL 2024.04-dirty (Sep 29 2025 - 13:52:40 +0800)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
SPL initial stack usage: 17064 bytes
Trying to boot from MMC1
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty
NOTICE:  BL31: Built : 04:20:32, Nov  1 2024

U-Boot SPL 2024.04-dirty (Sep 29 2025 - 13:56:05 +0800)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
Trying to boot from MMC1
Authentication passed
Authentication passed
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@23: Error reading output register


U-Boot 2024.04-dirty (Sep 29 2025 - 13:56:05 +0800)

SoC:   J722S SR1.0 HS-FS
Model: Texas Instruments J722S EVM
DRAM:  2 GiB (effective 8 GiB)
Core:  80 devices, 30 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Net:   Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@8000000port@1: phy_connect() failed
No ethernet found.

Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
Can't set block device
Failed to load '/boot/Image'
Failed to load '/boot/dtb/ti/k3-j722s-evm.dtb'
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Bad Linux ARM64 Image magic!
Scanning for bootflows in all bootdevs
Seq  Method       State   Uclass    Part  Name                      Filename
---  -----------  ------  --------  ----  ------------------------  ----------------
Scanning global bootmeth 'efi_mgr':
MMC: no card present
No EFI system partition
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@8000000ethernet@800000: phy_connect() failed
Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@8000000ethernet@800000: phy_connect() failed
  0  efi_mgr      ready   (none)       0  <NULL>
** Booting bootflow '<NULL>' with efi_mgr
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@23: Error reading output register
Loading Boot0000 'mmc 0' failed
EFI boot manager: Cannot load any image
Boot failed (err=-14)
Scanning bootdev 'mmc@fa00000.bootdev':
MMC: no card present
MMC: no card present
MMC: no card present
MMC: no card present
Scanning bootdev 'mmc@fa10000.bootdev':
Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@8000000ethernet@800000: phy_connect() failed
Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@8000000ethernet@800000: phy_connect() failed
Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@8000000ethernet@800000: phy_connect() failed