AM6442: Using GPIO1_18 (V1) and GPIO1_19 (W1) for Other Purposes When TimeSync Is Disabled (EtherNet/IP Adapter)

Part Number: AM6442


Tool/software:

We are currently working on implementing EtherNet/IP Adapter functionality on our custom board.

The PHY device we are using is .CUST_PHY_dp83867

For further background, please refer to the "Original question".

We are using a custom board based on AM64x and the Industrial SDK, and our implementation is based on a sample project provided in response to our "Original question".

On our design, GPIO1_18 (V1) and GPIO1_19 (W1) are needed for other purposes as general-purpose outputs (GPO).

However, these pins are assigned to SYNC and LATCH signals for the TimeSync feature, which creates a conflict.

Since we do not plan to use the TimeSync functionality, is it safe to repurpose GPIO1_18 and GPIO1_19 for other uses?

Are there any potential issues or side effects we should be aware of (e.g., PRU firmware behavior)?