This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM69: Technical Confirmation for Product Selection

Part Number: AM69
Other Parts Discussed in Thread: AM68

Hi team,

My customer is considering AM69 for their project.

They would like to confirm the following items.

Could you please help me ?

No.

Questions

1

Does the AM69x 4-core product lineup currently exist?

2

Is there anything you need to use the R core (e.g. provide a dedicated RTOS)?

3

Can I control the video output from the R core (at the level of writing the video to the framebuffer)?

4

Can you control PCIe from the R core?

5

Is the R core compatible with either big or little endian?

6

Is it Wayland (Weston) compatible?

7

Is X11 (X Windows System) supported?

8

Can RTOS be booted on each of the two R cores (can 3 OS be booted at the same time, including the a core)?

9

Are there any recommended JTAG debuggers?

10

Any Middleware Support for AM69x ?

 

Best regards,

Kenley