Hi,
Image color resolution not proper
I am using SBC8530 board (Processor DM37) and 7inch LCD. Using Windows compact 7 BSP version BSP_WINCE_ARM_A8 2.00.00.02. I have modified the lcd_vga.c file to suite the 7 inch LCD (800x 480). Width is set to 800 and height is set to 480 for default LCD parameter.
If I open a video or the jpg file the color resolution of image is not proper. Please see the attachment which shows the image captured from 7inch LCD and my laptop. The behavior is same for video file also.
LCD- 7 inch
LCD 7 inch
Laptop
Laptop
The same behavior is seen in the DVI output to the LED monitor. Please help me in resolving this issue.