This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Primary Boot mode from eMMC in Fs e secondary boot from SD

Part Number: AM625

Good morning,
On an AM6254-based board, I would like to have the following boot configuration: primary boot from eMMC in UDA File System and secondary boot from SD, also in File System mode.
The boot mode configuration should be:
Pin B7-B0: 01000011
Pin B15-B8: 00110110
Boot from eMMC works perfectly, but secondary boot from SD doesn't start. To test this, I removed the files from the eMMC memory so that the primary boot would fail, but the board didn't boot.
I did the same test, but configured the primary boot from eMMC in RAW using the dedicated boot partition, and both the primary and secondary boot from SD work, but I would like to use the eMMC in File System mode.
Is this a possible configuration?
Thanks for your attention.
Marco