This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MessageQ example program memory overlapped on C6A8168 EVM

Hi Todd,

I have another question regarding memory map of the two programs on DSP and ARM core. They look overlapped. For DSP the map is like this in message_dsp_x674.xdl

MEMORY

{

OCMC_0 (RWX) : org = 0x40300000, len = 0x20000

OCMC_1 (RWX) : org = 0x40400000, len = 0x20000

DDR_DSP (RWX) : org = 0x83000000, len = 0x2000000

DDR_SR0 (RWX) : org = 0x8e000000, len = 0x1000000

}

and for ARM the map is in the following in message_host_pea8f.xdl

MEMORY

{

SRAM (RWX) : org = 0x402f0000, len = 0x10000

OCMC_0 : org = 0x40300000, len = 0x20000

OCMC_1 : org = 0x40400000, len = 0x20000

VECTORS (RWX) : org = 0x0, len = 0x10000

DDR_HOST (RWX) : org = 0x80000000, len = 0xb000000

DDR_SR0 (RWX) : org = 0x8e000000, len = 0x1000000

}

I know these files are generated automatically and i cannot change them. But how do I control the memory map of those two cores, in the platform package file?

Thanks,

Zhao