Other Parts Discussed in Thread: OMAP-L138
Hi,
I am starting to work with OMAP-L138 experimenter kit. Specifically, I am evaluating the performance of C674x in terms of number of cycles this DSP needs to execute some algorithms.
With CCSv5.1, I have been able to connect to the target and load and run simple programs. But I am not managing to evaluate the number of cycles of a run of the code.
I have checked Run --> Clock --> Enable and Run --> Clock --> Show, and also set Run --> Clock --> Setup --> Count: CPU Execute Cycles.
Before running the code, I reset the counter to 0. What I am getting is a different number of cycles for every run: 1114 cycles for the 1st run, 2140 cycles for the 2nd run, 3166 cycles for the 3rd run, and so on.
Why is that?
On the other hand, if I use the simulator, I get always the same count: 34849 cycles, which is probably correct, taking a look at the generated assembler.
So, I think I am having the correct count with the simulator but not with the emulator. And with the emulator I have a different count for every run.
Does anyone have any ideas about why this is happening?
Regards,