Hi. I am using TI-EVM*DM8168
I upgraded my sdk from v5.00.00.11 to a newer one, with the following components:
arm_a8_codegen-2009q1_203/
bios-6.32.01.38/
dsp_c6x_codegen-7.2.5/
framework_components-3.21.01.26/
ipc-1.23.03.31/
linux-kernel-2.6.37-psp-04.00.00.12/
linuxutils-3.21.00.04/
osal-1.21.01.08/
syslink-02.00.02.80/
uia-1.00.01.17/
xdais-7.21.00.02/
xdctools-3.22.01.21/
I run the following commands:
1. insmod syslink.ko (load the syslink compiled for the linux kernel i am using)
2. ./firmware_loader 1 video.xem3 start
and the kernel craches with the following errors:
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
root@dm816x-evm:/opt/decoderSim# Unable to handle kernel NULL pointer dereference at virtual address 00000010
pgd = c0004000
[00000010] *pgd=00000000
Internal error: Oops: 17 [#1]
last sysfs file: /sys/kernel/uevent_seqnum
Modules linked in: syslink
CPU: 0 Not tainted (2.6.37 #2)
PC is at notify_shmdrv_isr_callback+0x1c/0xac
LR is at notify_shmdrv_video_isr+0x2c/0x3c
pc : [<c02a5c90>] lr : [<c02a5d88>] psr: 60000013
sp : c3b7fe88 ip : c3b7fea8 fp : c3b7fea4
r10: 00000004 r9 : c0061750 r8 : 00000004
r7 : 00000000 r6 : 00000000 r5 : 00000000 r4 : 00000000
r3 : 00000004 r2 : 00000009 r1 : 00000004 r0 : 00000000
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c5387d Table: 83b88019 DAC: 00000017
Process kworker/0:2 (pid: 45, stack limit = 0xc3b7e2e8)
Stack: (0xc3b7fe88 to 0xc3b80000)
fe80: 00000004 00000000 fffffffe 00000000 c3b7febc c3b7fea8
fea0: c02a5d88 c02a5c80 00000000 00000000 c3b7fee4 c3b7fec0 c03694cc c02a5d68
fec0: c04aaae8 c04aaadc 00000004 ffffffff 00000004 00000000 c3b7ff14 c3b7fee8
fee0: c00836d0 c03694a4 00000000 c04addb8 c3b7ff14 c3a90a00 00000004 c3b7ff34
ff00: c04addb8 c3864400 c3b7ff2c c3b7ff18 c0083708 c0083688 00000000 c04ade64
ff20: c3b7ff54 c3b7ff30 c0061798 c00836f4 c036952c 00000004 00000000 c3a90a14
ff40: c04ade64 c3ab4dc0 c3b7ff8c c3b7ff58 c0079a2c c006175c c3b7ff7c 00000000
ff60: c0078ac4 c3ab4dc0 c04addb8 00000009 c04addb8 c04addb8 c3ab4dd0 c3b7e000
ff80: c3b7ffbc c3b7ff90 c007a384 c007984c 00000000 c3b7ffcc c3831ee0 c3ab4dc0
ffa0: c007a1d0 00000000 00000000 00000000 c3b7fff4 c3b7ffc0 c007e684 c007a1dc
ffc0: c3831ee0 00000000 c3ab4dc0 00000000 c3b7ffd0 c3b7ffd0 c3831ee0 c007e5f8
ffe0: c006ace0 00000013 00000000 c3b7fff8 c006ace0 c007e604 ee40e382 40534013
Backtrace:
[<c02a5c74>] (notify_shmdrv_isr_callback+0x0/0xac) from [<c02a5d88>] (notify_shmdrv_video_isr+0x2c/0x3c)
r7:00000000 r6:fffffffe r5:00000000 r4:00000004
[<c02a5d5c>] (notify_shmdrv_video_isr+0x0/0x3c) from [<c03694cc>] (notifier_call_chain+0x34/0x78)
r5:00000000 r4:00000000
[<c0369498>] (notifier_call_chain+0x0/0x78) from [<c00836d0>] (__blocking_notifier_call_chain+0x54/0x6c)
[<c008367c>] (__blocking_notifier_call_chain+0x0/0x6c) from [<c0083708>] (blocking_notifier_call_chain+0x20/0x28)
r8:c3864400 r7:c04addb8 r6:c3b7ff34 r5:00000004 r4:c3a90a00
[<c00836e8>] (blocking_notifier_call_chain+0x0/0x28) from [<c0061798>] (mbox_rx_work+0x48/0xec)
[<c0061750>] (mbox_rx_work+0x0/0xec) from [<c0079a2c>] (process_one_work+0x1ec/0x318)
r6:c3ab4dc0 r5:c04ade64 r4:c3a90a14
[<c0079840>] (process_one_work+0x0/0x318) from [<c007a384>] (worker_thread+0x1b4/0x2d0)
[<c007a1d0>] (worker_thread+0x0/0x2d0) from [<c007e684>] (kthread+0x8c/0x94)
[<c007e5f8>] (kthread+0x0/0x94) from [<c006ace0>] (do_exit+0x0/0x5e4)
r7:00000013 r6:c006ace0 r5:c007e5f8 r4:c3831ee0
Code: e1a06000 f57ff04f e3a04000 e2843004 (e7960103)
FROM THE CODE I'VE BEEN ABLE TO SEE THAT THIS HAPPENS AFTER I CALL ipc_attach() function inside OMX_init() -> Domx_init() -> DomxCore_procInit() ->
any suggestions?