This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Are there any errors in SPI Module Registers Names?

Hello all,

I am trying to configure the SPI registers but there is conflict between SPI  module registers names defined in C5515 data sheet and the example in CSL library for C5515.

The example in CSL library csl_spi_example says that:

/* Send Read Status Command */
CSL_FINS(CSL_SPI_REGS->SPIDR2,SPI_SPIDR2_DATA,0x0500);
CSL_FINS(CSL_SPI_REGS->SPIDR1,SPI_SPIDR1_DATA,0x0);

But there is not any register description named SPIDR2 or SPIDR1 in the SPI  module registers names defined in C5515 data sheet. I think these two lines should be:

/* Send Read Status Command */
CSL_FINS(CSL_SPI_REGS->SPIDR2,SPI_SPIDAT2_DATA,0x0500);
CSL_FINS(CSL_SPI_REGS->SPIDR1,SPI_SPIDAT1_DATA,0x0);

Please correct me if I am wrong about this issue.
Regards.
***.