Hello ,
my question is about : what value to put in the SERDES configuration register in order to perform an internal loopback (i.e using PHY interface of the PCIE subsystem
implemented in TI product DSP C6678) .
Thank you very much
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ,
my question is about : what value to put in the SERDES configuration register in order to perform an internal loopback (i.e using PHY interface of the PCIE subsystem
implemented in TI product DSP C6678) .
Thank you very much
Hi, please refer to Section 2.11.2 PHY Loopback in the PCIe users guide (SPRUGS6A) for details on PHY loopback. The procedure is similar to PIPE loopback, but you also need to set both the Transmit and Receive paths in loopback mode to enable PHY loopback mode. These can be controlled in the SERDES Configuration Lane x Registers.
Also it is recommended to set loopback before link training. Otherwise, any transactions that were not looped back will cause sequence numbers to increment on transmitter but not on receiver. This will cause all following transactions to be dropped because of sequence number mismatch.
Yes i did that , but there is also no results . It is possible that we perform PHY Loopback without link training ?
Sorry, I did not quite understand "there are no results". Can you elaborate what it is that you observe? Let me get a PCIe expert to help you out.
i mean by " there is no results ", the fact of that no data is back to the Root complex after sending 1 data
The internal loopback in PCIe module seems not fully supported at this moment. And we are working on that to get more info.
Alternatively, we confirmed that the external loopback in PCIe module is working well in C66x devices.
On the hardware side, you need to connect PCIe pins externally, i.e. connect RXP pin to TXP pin, and RXN pin to TXN pin externally for Lane 0 (single lane testing) or for Lane 0&1 (two lanes testing). If you are using the C6678 EVM, you can have the TI AMC to PCIe card and have the external connection on the PCIe card edge or have other breakout card to get the connection ability of the PCIe pins.
On the software side, the initialization sequence mentioned in section 2.10.1.1 in PCIe user guide should apply to external loopback mode as well. It requires the PLL setup and link up training. The external loopback does not need special SerDes registers programming and it only applies to RC mode as well.
Please let us know if you have more questions about the external loopback and we will update you if the internal loopback is supported or not later. Thanks.
Sincerely,
Steven
Thank You Very much and i hope you arrive to perform the internal loopback quickly
For the other kind of loopback , i do not have a support to connect the 2 shannons , and i m afraid from doing it just with lanes welding ( RX1-- TX1 and RX2 --- TX2 ) , for
reasons of high frequency of transfer , fear of endommaging the two C6678 EVM platforms when welding , safety of platforms .....etc
So if you can adviser me of a method to connect the two shannons or to consolidate me of the safety of the previousely mentionned operation
Sincerely,
Younes
Younes,
If I understand correctly, you have two Shannon EVMs to be tested, right?
In that case, I think you could try the Dual EVM Break Out Card (CI2EVMBOC) for the two Shannon EVMs connection. You can find more info in the following page:
http://processors.wiki.ti.com/index.php/CI_Dual_EVM_Break_Out_Card
It could be ordered in TI estore and It supports the high speed interface communication like SRIO, PCIe, SGMII and AIF.
It should give you the solid connection between the PCIe peer-to-peer (RC-to-EP) connection. And the PCIe example in the MCSDK package can also be tested directly in this two-board setup.
And you could test more features in PCIe like configuration transactions, which is not supported in neither internal or external loopback mode. Hope it helps.
Sincerely,
Steven
Thank you very much Steven , realy you gived me interesting information ,
but actualy , i have to connect one C6678 and an other processor (FPGA), so the solution i need is not like the " Dual EVM Break Out Card "
so if you have any solution for me
Sincerely,
Younes
Younes,
If your FPGA board also has the PCIe male edge connector, you can use the TMDXEVMPCI on your C6678 EVM and plug both FPGA and C6678 into the PCIe backplane/motherboard which supports the communication between the boards. And you can set one as RC and another one as EP for the testing. There could be lots of choices on the market for the backplane/motherboard and you can do some research on that.
For the single board, external loopback testing, if you have concern about the safety/reliability issue, you probably can try the some AMC break out cards like the following one:
http://silicontkx.com/SMA-AMCULTRA9000.html
It gives you the capability of connecting each pins in the AMC connector of C6678 including PCIe pins and you can use SMA cables for the external loopback connection, which is reliable and easier for your testing.
Hope it helps.
Sincerely,
Steven
Steven,
I am doing something similar, connecting the C6678 EVM with an FPGA. I have the FPGA eval board with a male PCIe edge connector and wanted to use the TMDXEVMPCI for the C6678 to connect the two. I'm having a terrible time trying to locate a passive backplane that would allow the TMDXEVMPCI to be wired as an RC. From what I can tell, the TMDXEVMPCI is configured as an EP card.
Does TI have knowledge of a solution that allows the TMDXEVMPCI to act as the RC in a passive backplane? Or, am I missing something.
Thanks for your help.
Andrew,
I think you are correct that on the backplane, the PCIe slots are connected to the downstream ports of the PCIe switch on the backplane which are used for PCIe EPs.
I am not sure if the C6678 with TMDXEVMPCI could be plugged into the SHB/SBC slot and used as one host/RC. But it seems like the PCIe slots on the backplane are used for EPs only.
All,
There is some update for the PCIe internal loopback mode setup in KeyStone I devices. Please take a look and hope it is working for your testing with single EVM setup:
PHY loopback configuration for KeyStone I devices: