Other Parts Discussed in Thread: SYSBIOS
Hello:
I am trying to take "cc430x513x_dma_04.c - DMA0, Single transfer using ADC12 triggered by Timer_A0" example to uses the TI BIOS kernel. The BIOS setup HWI different than standard __interrupt void DMA_ISR(void).
Can some one shown me how to convert "cc430x513x_dma_04.c" DMA, ISR, and ADC to use the BIOS kernel?
Thank You
Mike
//******************************************************************************
// CC430x513x Demo - DMA0, Single transfer using ADC12_A triggered by Timer_A0
//
// Description: This software uses TACCR1 as a sample and convert input into
// the A0 of ADC12. ADC12IFG is used to trigger a DMA transfer and DMA
// interrupt triggers when DMA transfer is done. TA1 is set as an output and
// P1.0 is toggled when DMA ISR is serviced.
//
// ACLK = REFO = 32kHz, MCLK = SMCLK = default DCO 1048576Hz
//
// CC430x513x
// -----------------
// /|\| XIN|-
// | | | 32kHz
// --|RST XOUT|-
// | |
// | P1.0|-->LED
// | |
// | P4.1|-->TA1 output
// | |
// | P6.0|<--A0
//
// M. Morales
// Texas Instruments Inc.
// April 2009
// Built with CCE v3.1 Build 3.2.3.6.4 & IAR Embedded Workbench Version: 4.11B
//******************************************************************************
#include "cc430x513x.h"
unsigned int DMA_DST;
void main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Hold WDT
P1OUT = 0; // P1.0, P1.6 clear
P1DIR |= BIT0 + BIT6; // P1.0 output to LED, P1.6 GND
PMAPPWD = 0x02D52; // Get write-access to port mapping regs
P2MAP6 = PM_TA0CCR1A; // Map TA0CCR1 output to P2.6
PMAPPWD = 0; // Lock port mapping registers
P2DIR |= BIT6; // Output TA0CCR1
P2SEL |= BIT6; // Enable TA0CCR1 functionality
/* Initialize Timer A0 */
TA0CCR0 = 0xFFFE;
TA0CCR1 = 0x8000;
TA0CCTL1 = OUTMOD_3; // CCR1 set/reset mode
TA0CTL = TASSEL_2+MC_1+TACLR; // SMCLK, Up-Mode
/* Initialize REF module */
// Enable 2.5V shared reference, disable temperature sensor to save power
REFCTL0 |= REFMSTR+REFVSEL_2+REFON+REFTCOFF;
/* Initialize ADC12_A */
ADC12CTL0 = ADC12SHT0_15+ADC12MSC+ADC12ON;// Sampling time, MSC, ADC12 on
ADC12CTL1 = ADC12SHS_1+ADC12CONSEQ_2; // Use sampling timer; ADC12MEM0
// Sample-and-hold source = CCI0B =
// TBCCR1 output
// Repeated-single-channel
ADC12MCTL0 = ADC12SREF_0+ADC12INCH_0; // V+=AVcc V-=AVss, A0 channel
ADC12CTL0 |= ADC12ENC;
__delay_cycles(75); // ~75us shared ref. settling time
/* Initialize DMA0 */
DMACTL0 = DMA0TSEL_24; // ADC12IFGx triggered
DMACTL4 = DMARMWDIS; // Read-modify-write disable
DMA0CTL &= ~DMAIFG;
DMA0CTL = DMADT_4+DMAEN+DMADSTINCR_3+DMAIE; // Rpt single tranfer, inc dst, Int
DMA0SZ = 1; // DMA0 size = 1
__data16_write_addr((unsigned short) &DMA0SA,(unsigned long) &ADC12MEM0);
// ... from ADC12MEM0
__data16_write_addr((unsigned short) &DMA0DA,(unsigned long) &DMA_DST);
// ... to destination in RAM
__bis_SR_register(LPM0_bits + GIE); // LPM0 w/ interrupts
__no_operation(); // used for debugging
}
//------------------------------------------------------------------------------
// DMA Interrupt Service Routine
//------------------------------------------------------------------------------
#pragma vector=DMA_VECTOR
__interrupt void DMA_ISR(void)
{
switch(__even_in_range(DMAIV,16))
{
case 0: break;
case 2: // DMA0IFG = DMA Channel 0
P1OUT ^= BIT0; // Toggle P1.0
break;
case 4: break; // DMA1IFG = DMA Channel 1
case 6: break; // DMA2IFG = DMA Channel 2
case 8: break; // DMA3IFG = DMA Channel 3
case 10: break; // DMA4IFG = DMA Channel 4
case 12: break; // DMA5IFG = DMA Channel 5
case 14: break; // DMA6IFG = DMA Channel 6
case 16: break; // DMA7IFG = DMA Channel 7
default: break;
}
}