Unless I am overlooking something, I don't see a way for the GPIO lines on the C5502 to generate interrupts. Is this true?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mike,
I believe you are correct - GPIO does not have interrupt path to the C5502 DSP.
Pins INT[3:0] will interrupt the device. You also might be able to use timer input pin as interrupt.
Hope this helps,
Mark
Mark,
Mark Mckeown said:GPIO does not have interrupt path to the C5502 DSP
Wow. That's some pretty old silicon.....:)
Mark Mckeown said:Pins INT[3:0] will interrupt the device.
Unfortunately, the ezdsp5502 does not bring these pins out (INT0 & INT1) and uses the others for (INT2, INT3) I2C and Ethernet. I guess I'll have to add jumper wires to INT0 & INT1 and run them to the radio interface connectors (I'm migrating a project from C5515).