This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems about copying hua demo

Hi everyone,

    I imported the project hua_evmc6678l into CCS5.1 and rebuilt it, there wasn't any error.

However,if I copy the hua project  to another location(the linked files are copied,too ),

save it as a new project, modify the include options in project properties to be consistent

with the new project path,then rebuild it, there will be one error. It says :

xdc.tools.configuro: Error : Can't find platform package custom.hpdspua.evmc6678l.

How to eliminate the error? Any advice? The library version I use is

mcsdk_2_00_09_21 and pdk_C6678_1_0_0_21.

Hope someone helps. Thank you in advance.

Nuoxi

Best Regards