Hi,
I have a question about C6678 DDR3 I/F.
Is there any termination inside the C6678 DDR3.
In C6678 IBIS model, it is written like follow:
* Rx mode, 45 ohm Half Termination (90ohm to Vtt)
* Rx mode 50 ohm Full Termination (50ohm to Vtt)
Is this means that there are either 45 or 50 ohm termination inside the C6678?
best regards,
g.f.