What is the maximum capacity SD card that the 6748 supports? i see it supports high capacity cards so i am guessing it is more than 4GB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the maximum capacity SD card that the 6748 supports? i see it supports high capacity cards so i am guessing it is more than 4GB
If SDHC is supported it should support up to 32GB memory.
Please refer to the forum conversation on the thread here for details:
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/36575/128898.aspx
Regards,
Rahul