This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Change display resolution

Hi,

I'm running Android ICS (From TI-Android-ICS-4.0.3-DevKit-3.0.1) over an AM335x-EVM board. 

For testing purposes I'm trying to use a different display resolution using board's LCD panel. The resolution I would like to get is 320x240. I got it modifying $SOURCE_HOME/kernel/drivers/video/da8xx-fb.c at:

[2] = {
.name = "TFC_S9700RTWV35TR_01B",
.width = 800,
.height = 480,
.....

with

[2] = {
.name = "TFC_S9700RTWV35TR_01B",
.width = 320,
.height = 240,
.....

This is sufficient to get the display working at 320x240 on a limited area of it (that is what I want).

Another thing I've done is to modify all "WVGA" occurrences in "board-am335xevm.c" with "QVGA" but it seems not to be influent.

I've also changed lcd density adding "ro.sf.lcd_density=120" in build.prop.

 

The problem I'm facing is that quite every application I start is crashing, for example if I start Settings application the result is attached here: http://pastebin.com/ydtkwCFs

Do someone have an idea for this?

Thanks,

Francesco