Hi, is just that i am working with a device based on OMAP4430/4460, and i am running Android ICS on it, and when i run the O.S. on it, it has an ID number named androidboot.serialno, it is a serial number and it also appears when i flash the SD card for the board (pandaboard), and that id always changes for different boards, but each board has its own number, so i would like to know where does that serial number come from, does it come from the OMAP4430/4460? because as far as i know, the board doesn't bring any memory, so, i need to know where does it come from for me to use that number.
Best Regards.